Part Number: TVS1800 Other Parts Discussed in Thread: INA592 , , TVS3300 Hi Team,
We need to add some protection to our 36V OPAMP such as INA592. The datasheet for INA592 states maximum is +/-18 or 36V.
While the datasheet for TVS1800 shows it doesn…
Part Number: TVS1800 Other Parts Discussed in Thread: TPS25947 Hi team,
I consider using TVS1800 as transient surge protection for TPS25947 input line (absolute maximum rating <28V).
According to datasheet, TVS1800 can clamp voltage below 23.4V…
Hi Yu-Chen,
Find below a table with measured values for the forward voltage, breakdown voltage, clamping voltage, and IPP. For the TVS3301 the forward voltage of the device was not tested and is also not included in the datasheet. The DC breakdown current…
Part Number: TVS1800 Team,
I find that most of our surge protection deives can achieve 1kV protection. Do we have cost down version that can just achieve 200V protection? Is TVS1800 the cheapest one?
Regards,
Nic
Part Number: TPS2663 Other Parts Discussed in Thread: TPS1686 , TPS25983 , TPS25947 , TVS1800 , TVS2200 Tool/software: hi, We are working on a design related to eFUSE and hope that the rated output can reach 10A. As TPS1686 cannot be ordered yet, we would…
Part Number: TVS3300 Other Parts Discussed in Thread: MCT8329A , TVS1800 Tool/software: Hello,
I need the device with flat clamp at 60V, something like TVS3300 but for 60V and about 30A.
I can have a margin of 58-62V.
Can you suggest simplest possible…
Part Number: TPD1S414 Other Parts Discussed in Thread: TVS2200 , TVS1800 , , TPD1S514 Tool/software: I have a customer designing a high volume product with USBC, but only 5V VBUS (no PD). They would like to protect against the case of a non-compliant…
Part Number: LM74703-Q1 Other Parts Discussed in Thread: TVS1800 ,
Tool/software:
Hi TI,
Why for 24V battery protection application 58V TVS diode is recommended? Does not such diode have typical clamping voltage of over 90V which far exceeds LM74704…
Hi Mitchell,
TVS1800 is a unidirectional device, so if your application requires negative signals, it would clamp those negative sections and kill the signal.
If you like the performance of TVS1800, we have TVS1801 which is bidirectional and offers…