Part Number: TVS-RECOMMENDATION-CALC Other Parts Discussed in Thread: TVS2701 Hello, I wanted to know if there is any unencrypted spice model for the TVS2701 as I am using LTSPICE
Part Number: TVS2701 Tool/software: Hi team,
In "12.2 Layout Example" of the datasheet, the width of the power supply trace seems to be the same length (0.6mm) as the PAD of the IN terminal of the TVS2701.
If the trace width is 0.6mm, the current…
Part Number: TVS2701 Tool/software: Dear Support,
Can you tell how to properly Fuse the TVS2701 TVS diode ?
Vin normal operation 24V 1.25A -> 30W , max current 2.25A -> 54W
Can you tell how to size the fuse, so that the fuse blows before the…
Part Number: TVS2701 Tool/software: These days I'm in an external laboratory to do the EMC and RED tests on our new industrial gateway to release the CE certify and I need to close the activity in the next few days.
I put below the schema and the lay…
Part Number: TVS2701 Other Parts Discussed in Thread: TVS2201 , STRIKE Hi Team,
we are currently using the following scheme for reverse polarity where TVS is after RPP.
The input is 24VDC from standard industrial supply.
But now we want to…
Part Number: TVS2701
Dear Technical Support Team,
I got TVS2701DRBR and this marking is "PPTP".
Is this correct marking? Is this fake chip?
According to the datasheet, the marking of T VS2701DRBR i s "1PTP".
Best Regards,
ttd
Part Number: TVS2701 Other Parts Discussed in Thread: TVS3301 Hello,
I would like to simulate TVS2701 and TVS3301 on LTSpice, and thus need the SPICE model.
The one available to download from the TI website is encrypted, can I get a model that is…
Part Number: TVS2701 I want to recommend TVS2701 to customer and replace 3.0SMCJ26CA-AU_R1_00001,SMC ! Please help to confirm if there is an error ,THX
Part Number: TVS2701 Hi team,
One of my customer considers to use TVS2701 and provided a question.
The datasheet’s layout example shows that input trace width seems to be same as input lands.
Is there concern that trace width which is wider…
Part Number: TVS2701 Hi,
I am developing a device which need protection according to MIL-STD-1275E: everyspec.com/.../download.php
The device need to withstand a 100V surge and a ±250V spike. I have found a solution to withstand the 100V surge test…