Part Number: TVS3300 Hello TI Team,
I am currently using the TVS3300 in one of our projects. Based on the transient analysis simulation, the peak power dissipation is estimated to be 20.5W [TD = 450ns] .
Could you please confirm whether the TVS3300…
Part Number: TVS3300 Other Parts Discussed in Thread: TVS3301 Tool/software: Hello TI Team,
Could you please help me understand the behavior and performance of the TVS3300 & TVS3301 during negative transients according to ISO7637-2? Do we have any test…
Part Number: TVS3300 Other Parts Discussed in Thread: STRIKE Tool/software: Hi,
is the maximum voltage for IEC 61000-4-2 the same as for IEC 61000-4-5 ?
Often -2 ist higher than -5.
Does the spice model include this and if so can you send us an…
Part Number: XTR300 Other Parts Discussed in Thread: TVS1400 , TVS3300 , TVS0500 , TVS1401 Tool/software: Hi dear,
I would like to be sure which could be the best solution to protect XTR300, so, the power supply should be 24 V DC and -5 V DC, so I read…
Part Number: XTR300 Other Parts Discussed in Thread: TVS3300 , Tool/software: Hi all,
I would like to know how protect the output XTR300 in current and voltage mode. The power V+ should be 24 V DC and V- should be -5 V DC. So, I've read that the two…
Part Number: TVS3300 Tool/software: Hello, my customer can only find the length and wideness of TVS3300DRVR, and they want to know the height of TVS3300DRVR. Could you please provide with specific height data? Thanks a lot!
Part Number: TVS3300 Hi Experts
Can someone provide an unencrypted spice model for TVS3300?
You can email me at jim.brinkhurst@ti.com .
The customer is Northrop Grumman Space, and we do have a current NDA with them.
Best regards,
Jim B
Part Number: TVS3300 Hello guys,
One of my customers is looking for surge protector for DCDC converter connected to 24V motor VM (motor power supply terminal).
The motor generates up to 30V to VM as back electromotive force. Also the current is up…
Part Number: TVS3300 Other Parts Discussed in Thread: MCT8329A , TVS1800 Tool/software: Hello,
I need the device with flat clamp at 60V, something like TVS3300 but for 60V and about 30A.
I can have a margin of 58-62V.
Can you suggest simplest possible…
Part Number: TVS3300 Other Parts Discussed in Thread: TVS2700 , TVS2701 Tool/software: Input Voltage is of 28V and current is 2A. Power Module Voltage Range: -1V to 6V
Which is the best method to be followed:
Reverse.tif
Kindly suggest TVS diode…