Part Number: TVS3300 Hello,
I'm thinking of use two TVS3300 in a parallel to achieve a higher current capability. I know that is very hard to achieve a true current sharing because of even a little breakdown voltage difference between two diodes. Additionaly…
Part Number: TVS3300 Other Parts Discussed in Thread: LMR36506 , , TVS2700 , INA229 , ATL431LI
I have an application where I have a working voltage of 3V to 60V (up to 65V preferred) and a max clamping voltage of 70V. It will be used to protect the input…
Part Number: TVS3300 Hi team,
Could you tell the failure mode of TVSxx series? Is that Short?
When customer expect it will be short, are there any way to fill the gap?
Regards,
Noriyuki Takahashi
Part Number: TVS3300 Other Parts Discussed in Thread: STRIKE Hi,
My customer run ESD test and compare the result among TVS diode and TVS3300.
Test Condition:
TVS diode test result
TVS3300 test result :
IN voltage of TVS3300 reduce soon after attaching…
Part Number: TVS3300 Other Parts Discussed in Thread: STRIKE Hi, We see that TVS3300 is used for 8/20us surge protection application. We have requirement to protect circuit from 10/350us surge.
To know 10/350us surge, Please refer ntsa.co.za/.../
in this…
Part Number: TVS3300 Customer requested,
Could you parallel multiple devices to support larger surge currents?
Not sure how fast the Flat Clamp devices start conducting, if faster then the current increases (us-range) then I'd expect it could be an option…
Part Number: TVS3300 Other Parts Discussed in Thread: TVS3301 , TVS1400 , TVS0500 Hello,
I would like you to confirm about EMC test condition for this device.
* According to datasheet, there is following description.
"TVS3300 has been tested according to…
Part Number: TVS3300 Other Parts Discussed in Thread: CSD18510Q5B , LM74700-Q1 , , TVS3301
I am planning on using a TI LM74700-Q1 ideal diode controller to control a TI CSD18510Q5B power MOSFET to protect a PCB with up to 28V input, at up to 15A continuous…