Part Number: TVS3301
Hello support team,
My customer inquires TVS3301 parallel usage. Could you support?
*TVS3301 has 1kV/1100W capability for 61000-4-5. If they put two parallel TVS3301, can these two consider to support 2200W?
*They assume…
Part Number: TVS3301 Other Parts Discussed in Thread: LM5176 , , TSM36A Hi,
I would like to use this to protect a LM5176. The latter is spec'd to 60V to input range so in terms of clamping voltage the TVS3301 will do a great job. However, I would prefer…
Part Number: TVS3301 Other Parts Discussed in Thread: TVS2700 , TVS2701 , TVS3300 , Hi there, we have two protection applications:
Application 1: DC Input
Working voltage: 28V
AMR of device we are protecting = 40V - clamping voltage should be…
Part Number: TVS3301 Hello guys,
One of my customers is considering using TVS3301 to protect for 30V line of their new products.
They have a question as the follow. Could you please give me your answer?
Q. What level is TVS3301 categolized to in…
Part Number: TVS3301 Other Parts Discussed in Thread: TVS3300 , Hi,
Can you suggest me an alternate for this
The standoff needs to be same
the max voltage should be 40V
should pass IEC 61000-4-5 (8/20 µs) at 500V 250A
Part Number: TVS3301 Other Parts Discussed in Thread: TPD1E10B09 , TVS3300 Hi team,
is there a TI alternative to Vishay's VCUT0714A-HD1-GS08?
what would be the closest device?
Thanks,
Kevin