Part Number: TX7516EVM Other Parts Discussed in Thread: TSW14J50EVM , AFE58JD18EVM , , TX7516 , TX75E16 I currently own afe58jd18evm and tsw14j50evm. I heard TX7516EVM is scheduled for obsolescence . Any alternative that is compatible with my existing…
Part Number: TX7516EVM Other Parts Discussed in Thread: TX7516 Hi,
I have a few questions in terms of communication between Tx7516 EVM board and our PC:
1) how to write to delay register through python(how to interpret addr, val in writeReg or delayWriteReg…
Part Number: TX7516EVM Tool/software: Hello,
I've attempted to install and run the Latte GUI (v1.4) for the TX7516EVM but am running into the following problem when I try to run the installed application:
Windows PowerShell Copyright (C) Microsoft…
Part Number: TX7516EVM Tool/software: Hi. I'm experiencing an issue with the TX7516EVM. When I switch the board from transmit mode to receive mode via the T/R switch, I notice that the received signal exhibits significant high frequency noise, which is…
Part Number: TX7516EVM Other Parts Discussed in Thread: TX7516
hi
using the EVM for TX7516 the reference Clock is fixed in the factory default 156.25Mhz. On the EVM software we do have a LMK61E2-SIAR dropdown control, but it is not seen to generate…
Part Number: TX7516EVM Hi,
I just started working on the TX7516EVM and were following the user guide.
I set the power supplies as specified on the user guide and the +5V supply showed 2Vdc & 200mA.
I’ve sprayed some freeze spray on the eval board…
Part Number: TX7516EVM Other Parts Discussed in Thread: TX7516 Hi Experts,
Seeking your confirmation please:
We wonder if we use a TX7516EVM as a transmitter to evaluate an ultrasound probe, do I need to buy another receiver EVM to cooperate with…
Part Number: AFE7960EVM-DOC-CERT Other Parts Discussed in Thread: TX7516EVM Hi.
I have the TX7516EVM kit and as part of my evaluation I need to control the Latte GUI from Matlab.
TI provides a python script to facilitate connection to the Latte server…
Part Number: AFE58JD18EVM Other Parts Discussed in Thread: TX7516EVM , TSW14J50EVM , TX810 Tool/software: I am developing ultrasound probe. To generate pulse for and analyze signal from the developed probe, I have purchased tsw14j50evm, tx7516evm, and…
Part Number: AFE58JD48EVM Other Parts Discussed in Thread: TX517 , TX7316EVM , , TSW14J50EVM , TX7516EVM , AFE58JD28EVM Tool/software: Dear TI Team,
I am currently working on developing an ultrasound imaging system using TI’s EVMs. Based on information…