Part Number: TXB0102
In this schematic diagram, when the VCCB outputs a high level, T1 conducts. What is the current loop of the internal 4K resistor, and why is it recommended to pull up or down resistors above 50K.
Part Number: TXB0102 Hello,
I am contacting you to ask about the transistor count on TXB0102DCUR. We need this for the SR-332 standard, so an approximate count will work for us.
Thanks
Part Number: TXB0102 Other Parts Discussed in Thread: TXS0102 Hi Team,
I was planning to use the TXB0 series level translator in the design.
The TXB0102 is an auto-direction level translator intended for push-pull buses. However, it is generally not…
Part Number: TXB0102 I am currently using TXB part level translator in my design here in datasheet it is mentioned as VCCA must be lesser than VCCB, but in my design i have given VCCA greater than VCCB, as a result i am not getting one of the output can…
Part Number: TXB0102 Other Parts Discussed in Thread: TXU0101 Hi Team,
We are using the TXB0102DCUR IC as a 5 V to 3.3 V level translator. In our design, R286 is populated with a 100 k pull-down resistor, while R288 is DNP.
The measured voltage levels…
Part Number: TXB0102 Hi Sirs,
Current project have use TI.TXB0102 to achieve general I/O bi-directional and voltage transfer from low (1.8-V) to high (5.0-V) level convert case, here is my design schematic be reference.
After review the datasheet…
Part Number: TXB0102 Other Parts Discussed in Thread: TXB-EVM Tool/software: I would like to simulate the TXB0102DCUR which is bidirectional voltage level shifter it is not available in Pspice for simulation. It only has IBIS model can you able to provide…