Part Number: TXB0102 Other Parts Discussed in Thread: TXU0202 Hello,
My name is Amith. I am using your component TXB0102 in my circuit as a voltage level converter for UART data lines from 3.3V to 1.8V and opposite directions.
My connection configuration…
Part Number: TXB0102 Other Parts Discussed in Thread: TXU0202 Hello Dear,
I want to use TXB0102 as level shifter for uart application.
Is TXB0102 suitable for Uart aplication?
Part Number: TXB0102 Other Parts Discussed in Thread: MSP430FR2433 I'm using the TXB0102 and seeing noise that prevents using it above ~1MHz, but the datasheet claims 60 MHz (60 Mbps) for my VDD setup.
In the attached scopeshots, a 2MHz square wave…
Part Number: TXB0102 Other Parts Discussed in Thread: TXB0302 , TXU0304 , TXU0104 , TXU0204
Hello dear support community,
Everything is in the title, could you please explain me what is the difference between TXB0102 and TXB0302 components please ? I could…
Part Number: TXB0102 Other Parts Discussed in Thread: TXU0102 , SN74LXC2T45 Hi there. I'm looking for a level shifter/buffer for an SPI master running at 1.8V to 8 slaves at 3.3V. And in a package rated for 125C. Individual OE control by the Master…
Part Number: TXB0102 Other Parts Discussed in Thread: TXS0102 , LSF0102 Regarding the Voltage Level Translator (TXS0102 / TXB0102 / LSF0102) ,
in case supply voltage is supplied to the VccB(or Vref_B) port and is not supplied to the VccA(or Vref_A) port…
Part Number: TXB0102 Other Parts Discussed in Thread: TXS0102 , TCA9406 Hello,
I'm looking for P2P replacement of ET2102 from ETEK. Please find the link : http://www.etek.com.cn/en/product.asp?id=327
ET2102 is auto bi-directional I2C level shifter…
Part Number: TXB0102 In datasheet, mention OE pin must be pulldown.
But I did an experiment about OE pin is without pulldown, then this experiment does not affect the function.
So if I don't have pulldown on OE pin, it will have side effect?
Part Number: TXB0102 Other Parts Discussed in Thread: SN74AXC2T245 TXB0102 for UART Application
TXB0102 is used for UART translation usually. Will following scenario cause some problem?
Power on the target board first, VCCA and VCCB are supplied.
Then…
Part Number: TXB0102 Other Parts Discussed in Thread: SN74LVC2T45 , TXU0204 , SN74AVC2T245 , SN74AXC2T245 , TXU0202
Hello, I am searching for a 2-bit interface solution, unidirectional, dual power source, non-autosensing, Push-Pull, for UART and for proprietary…