Part Number: TXB0104-Q1
Hi team
Are there any level shifter recommendations similar to TXB0104Q1 with B port Cin less than 10pf and we need automotive level device, thank you.
Part Number: TXB0104-Q1 Other Parts Discussed in Thread: TXS0206 , TXS0108E-Q1 , TXS0108E Hello:
We now use TI chip txb0104qrgyrq1 as the level conversion chip. The schematic diagram is as follows. There are several points in the schematic diagram that…
Part Number: TXB0104-Q1 Other Parts Discussed in Thread: TXB0104 , TXU0304 , TXU0104 , TXU0204 Hi team,
My customer want to use TXB0104-Q1 for functional safety system design. Could you please help to check whether we can support these documents?
…
Part Number: TXB0104-Q1 Other Parts Discussed in Thread: SN74AXC4T774-Q1 , Hi expert,
Do we have another device which no limited on VCCA≤VCCB? This voltage translator uses for SPI voltage translated from 3.3V(power1) to 3.3V(power2) and in automotive…
Part Number: TXB0104-Q1 Other Parts Discussed in Thread: TXB0104 , Hi team,
Customer get an urgent question as below. Can you please feedback ASAP? Thanks!
Their working conditions is, VCCA keep 3.3V, while VCCB would drop to 0V when system is in…
Part Number: TXB0104-Q1 Hello team,
A customer uses TXB0104-Q1 to translate1.8V to 5V, but the OE is connected to VCCB.
-. Is it okay?
-. The datasheet recommends that OE input circuit is supplied by VCCA. Can you explain why it recommends VCCA…
Part Number: TXB0104-Q1 Other Parts Discussed in Thread: SN74LVC2T45-Q1 Dear all,
i need to connect 2 different boards by a 40cm long cable. The communication interface is SPI.
Inside the board the voltage level is 3V3 and for transmission 5V is used…
Part Number: TXB0104-Q1 Hi experts,
May I know the reason of why "When the output-enable (OE) input is low, all outputs are placed in the high-impedance state." ?
Which part is the +/- 2mA in 8.3.2 driving?
Is this 4kOhm a real resistor or a equivalent…
Part Number: TXB0104-Q1 Hi Sir,
I am looking for ADG3304WBRUZ automotive part pin to pin replacement.
Do you think TXB0104QPWRQ1 is good option? Any design caution if change to our part?
Or there is other good recommendation?
Thank you.
Regards…
Part Number: TXB0104-Q1 Other Parts Discussed in Thread: LSF0108-Q1 , SN74AXC4T245-Q1 , SN74AXC4T774-Q1 , SN74AXC4T774 , SN74AXC4T245
Hi team,
we are using your level shifter TXB0104QPWRQ1 for 1.8V to 3.3V convert, but we find the waveform have some…