Part Number: TXB0108 Other Parts Discussed in Thread: SN74AXC8T245
Hi team,
We are currently evaluating the W25Q32RVNJQ SPI NOR Flash with an FPGA using a Xilinx XMC-105 debug card.
The FPGA QSPI interface operates at 1.8 V, while the flash device…
Part Number: TXB0108 For the TXB0108 bidirectional voltage level translator our plan was to use the B side as an 5V TTL input and A side as a 1.8V logic output. For most situations the B side will see a logic level high or low. However when the device…
Part Number: TXB0108 Hi Experts,
We are performing a SI simulation on a board that includes the TXB0108DQSR IC. During the simulation, we are observing non-monotonic behavior in the waveform.
The issue occurs specifically when using the txb0108.ibs…
Part Number: TXB0108 Other Parts Discussed in Thread: TXS0108E , Hi Team,
We are using TXB0108DQRS part in our board. we are doing signal integrity analysis for it. here, we are observing non-monotonic behaviour in our waveform.
This issue was raised…
Part Number: TXB0108 Other Parts Discussed in Thread: TXB-EVM , TXS0108E Hi Experts,
We are performing a SI simulation on a board that includes the TXB0108DQSR IC. During the simulation, we are observing non-monotonic behavior in the waveform.
The…
Part Number: TXB0108 Other Parts Discussed in Thread: TXB0604 , TXS0108E Hi,
We have used TXB0108 bidirectional buffer in 1.8V logic (Vcca & Vccb). In the datasheet for Vcca & Vccb = 1.8V, the maximum data rate supported is 52Mbps. Our SPI clock is…
Part Number: TXB0108 The semiconductor feature size for the TXB0108PWR is needed in nm. The smallest gate length in nm is the dimension of interest for transistor and MOS devices.
Part Number: TXB0108
Tool/software:
I have a query regarding the MPN: TXB0108 8-Bit Bidirectional Voltage-Level Translator . There appears to be a discrepancy between the Top View diagram on Page 3 and Section 4.1 on Page 5 of the datasheet, specifically…
Part Number: TXB0108 Tool/software: Hi Team,
We are using TXB0108 in our design. We have connected open drain pin in this level translator with the pullup of 2.2K. Functionality side we are not facing any issue. It is working fine. But in datasheet…
Part Number: TXB0108 Hello team,
We are using TXB0108 level shifter in our application inbetween CPLD and D type flip flop.The CLD is operating at 3.3V logic and D type level shifter operating at 5V logic .The signal we are expecting is bidirectional…