Part Number: TXB0108TXB0108RUK datasheet does not state the pinout for this package. On one datasheet it has 6 pins on two sides and 4 on the other two sides. However it then shows the package information as 5 pins on each of the 4 sides in the WQFN…
Part Number: TXB0108 Tool/software: Dears,
The customer uses a level conversion chip, and the specific application is to realize PBI bus communication between DSP F28377D and a communication board. Now I want to choose a bidirectional level conversion…
Part Number: TXB0108 Hi Team,
I am currently evaluating the TXB0108 8-bit bidirectional voltage-level translator for an upcoming board design. During component selection, I noticed two distinct orderable part numbers for the DSBGA package: TXB0108YZPR…
Part Number: TXB0108-Q1 Other Parts Discussed in Thread: TXB0108 , Dear expert,
Customer have concerns on using 1.2V to 1.8v/3.3v as mininal VCCA 1.2V use case. especially on high tempreture and low tempreture which may in unstable status. Need your…
Part Number: TXB0108 Other Parts Discussed in Thread: TXU0304 , TXU0104 , TXU0204 Tool/software: Dears,
My customer use our TXB0108. The DSP signal level is 3.3V, and the MVB board signal level is 5V. TI's TXB0108pwr level conversion chip is used…
Part Number: TXB0108 Hi,
Initially, I evaluated the level shifter’s compatibility with the memory interface based on voltage levels and data rate. Are there other electrical characteristics I should consider that could impact compatibility between the…
Part Number: TXB0108 Other Parts Discussed in Thread: TXS0108E
Hi Exerts,
We'd like to ask the following operation if applicable:
I have bidirectional 5V CPCI signals which need to be level translated to 3.3V CPCI signals. I can see below parts…
Part Number: TXB0108 Tool/software: Hi team,
Could you please help share the Vo and Io output curve of TXB0108.
Customer wants to use it output 50mA current. Is it ok?