Other Parts Discussed in Thread: TXB0104-Q1 , TXB0108-Q1 Hello,
What is the maximum frequency it can handle? for below parts -
SN74AHC125QPWRQ1, TXB0104-Q1, TXB0108-Q1, TXU0304QPWRQ1
Regards,
Amol
Part Number: TXS0108E-Q1 Other Parts Discussed in Thread: TXS0108E , TXB0108 , TXB0108-Q1 Hi
I am using TXS0108E-Q1 part in my application.Few I/O lines are unused so do i need to pull it to respective Vcc or GND?
Regards
Nitesh
Part Number: TXB0108 Other Parts Discussed in Thread: TXB0104-Q1 Hi,
I found TXB0108 Driving current is not enough for my application.
I found TXB0104-Q1 seems can support to 40uA.
Do you have any better suggestion?
Thanks!
Jeff
Part Number: TXB0108 Other Parts Discussed in Thread: TXU0304-Q1 , TXU0104-Q1 , TXU0204-Q1 Hi team,
Do we have the TXB0108 for vehicle?
Whether or not in the plan
Part Number: TXB0108 Hello guys,
One of my customers is going to use TXB0108 with the following connection.
CPU output pin(3.3V, Io=+/-4mA) -> TXB0108(side B, 3.3V) -> TXB0108(side A, 1.8V) -> TXB0108(side A, 1.8V) -> TXB0108(side B, 3.3V) -> CPU…
Part Number: TXB0108 Other Parts Discussed in Thread: SN74HCS125-Q1 Hi, I’m working with a 3rd party device which contains a TXB0108 bidirectional voltage level translator. It is used, likely inappropriately, to drive GPIO signals to components external…
Part Number: TXB0108 Hello guys,
One of my customers is considering using TXB0108 for their next products.
They have the following questions about TXB0108. Could you please give me your answers or comments?
Q1. Is there any ESD protection diode…
Part Number: TXB0108 Other Parts Discussed in Thread: LSF0108-Q1 , SN74GTL2003 , SN74LVC8T245 Hello,
I am looking for an octal bidirectional level shifter 3.3V TTL to 5V CMOS.
For reliability issues (the IC will be used in a measurement instrument…
Part Number: SN74AXC8T245 Other Parts Discussed in Thread: SN74LVC8T245 , , SN74LVC2T45 , SN74LVC16T245 , LSF0108-Q1 , TXB0108 , LSF0108 , SN74LV4T125 , CD40109B Hey Guys,
I made a terrible mistake: I use the SN74AXC8T245PW in my design and reconfigured…
Other Parts Discussed in Thread: TXB0108 , SN74AVC16T245 , TXS0102 , SN74AVC16T245-Q1 Hi everyone,
I need a level shifter for a RMII bus. Bus contains one 50 MHz clock, and data signals that are synced with 50 MHz clock. Voltage of PHY side is 1.8V…