Part Number: TXB0304 Other Parts Discussed in Thread: TXB0104-Q1 Tool/software: Hi
Could you please help confirm whether there are any materials with the same specifications as the following materials and working temperature of -40~125°C that can be…
Part Number: TXB0304 Other Parts Discussed in Thread: TXU0204 Tool/software: Hi Support Team,
I encountered an issue while using TXB0304RUTR and would like to request your assistance. I need to convert a 3.3V signal from a GNSS Module to a 1.8V signal…
Part Number: TXB0304 Hi team,
Customer want to use TXB0304 reach >100bps with 1.8V to 3.3V.
For high Cap load situation, could we use multi-channel in parallel to get higher drive strength and realized higher data rate?
BR,
Victor
Part Number: TXB0304 Hi sir,
Is the TXB0304 data translation A1<-->B1, A2<-->B2, A3<-->B3, A4<-->B4 or like the datasheet described A1(input/output1)<-->B4(input/output1) ?
Thanks a lot.
Part Number: TXB0304 Tool/software: Hello team,
Should I tie the output of the unused ports to GND?
My customer has tied the inputs to GND, but they have observed oscillation at the output.
Best Regards, Kei Kuwahara
Hi team,
Could you please recommend eSPI redriver(50MHz, 4channel)? If we have, what's the layout requirement for this device? Close to TX or close to RX?
Part Number: TXB0304 Other Parts Discussed in Thread: TXU0102 Hi
Customer measurement found that U22 PIN8 has an abnormal waveform when USB is abnormal (USB_OC#_abnormal.png) U22 uses TXB0304RUTR
Changing RA43 to a smaller size (1K for testing) can…