Part Number: TXB0304 Dear TI team,
I'm using IBIS model in HSPICE and encountering error : "**error** (b_lvlshftd:15) Buffer is power on with voltage source connected to node PU, where File = txb0304.ibs, Model = IO_33_OS"
Seeking for the right…
Part Number: TXB0304
I am trying to simulate a non-standard SPI implementation in ADS with the TXB0304RSVR.
The SPI consists of 3 signals (SS, CLK, MISO/MOSI), where the MISO and MOSI are shared on a single line, hence the need for a bi-directional…
Part Number: TXB0304 Other Parts Discussed in Thread: LSF0204 , TXU0304 , SN74LVC125A Hi,
I am designing a system that has lot of slave devices running on a single SPI bus. The architecture of the existing system is represented in the attached image…
Part Number: TXB0304 Other Parts Discussed in Thread: TXB0302
Dear TI Expert,
When using TXB0304, we are a bit confused with the datasheet description, which seems to have a conflict between two screen shot below and related description section, so…
Part Number: TXB0304 Hi,
I am using the mentioned part number (TXB0304RUTR) level translating for push pull configuration, so I would like to know about the switching frequency of the mentioned level translator.
Thanks,
Nandhini A.
Part Number: TXB0108 Other Parts Discussed in Thread: LSF0108 , , SN74AXC1T45 , SN74AXC8T245 , SN74AXC4T774 , SN74AXC4T245
Hi team,
My customer mow is using NXP's NXB0108PW.
And now they have a test condition: 5 ns voltage pulse.
Could you please…
Part Number: TXB0304 Hi,
My customer design VCCA and VCCB both are 1.8V. If they want to evaluate/qualify delay time, which row they should refer to?
BTW, is CL mean trace length?
Part Number: TXB0304 Hi team,
We see 2 kinds of pin 1 in RUT package, L option and Δ option. Could you please let me know which is the default? and how to order the other type when needed?
RUT0012A RUT (R-PQFP-N12) 4220310 (Rev. C) (ti.com)
Best…
Part Number: TXB0304 Other Parts Discussed in Thread: TXU0304 , TXU0104 , TXU0204 Hi:
we experience SPI voltage drop while using TXB0304RUTR as the voltage translator
The voltage drop is due to load capacitance higher than spec (100pF)
There…
Part Number: TXB0304 Hi team,
A customer of mine is looking to use TXBN0304 and powering VCCA with 1.8V. Is it violating specs to apply 3.3V to OE or OE"not" depending on which device they select?
Thanks!
-Will