Part Number: TXS0206 Dear Team,
Do we have any SD 3.0 buffer or driver solution as the following requirements. Thanks.
- Support SDR104 mode, clock rate 208MHz
- Support DDR200 mode, clock rate 200MHz
- Trace length 250mm
Many Thanks
Jimmy
Part Number: TXS0206
Hi team,
My customer is considering to use the TXS0206. The condition is VCCA=3.3V and VCCB=1.8V.
The customer would like to know the tpd minimum value of CLK and DAT. I know that the minimum value has not been tested, but could you…
Hi Dylan:
Thank you for all your help. I have tested the device and it works great, with wires up to 40cm (did not test longer). Thank you for your help. For anybody in the future that needs a similar application, this is a good solution. You can tie…
Part Number: TXS0206 Hi team,
My customer is considering to use TXS0206. Could you answer to the question below?
When the voltage is applied to VCCA and no voltage is applied to EN and VCCB, will the output of B-side terminals (CLKB, CMDB, DATAB) become…
Part Number: TXS0206-29 Hi Team,
Help to check the dimension size in data sheet P.24. Will it be ok if customer use 1.558 mm for E? =(1.588+1.528)/2.
Per customer feedback, the CAD limitation would be down to 3rd digits after decimal. it would be an issue…
Part Number: TXS0206 Dear,
Here we have a need for level shift in SD application. The voltage level in AP side is 1.8V, in SD side is 3.3V. It needs to support SDR104 standard, do we have such devices? Thanks.
And do we have a mapping table about SD…
Part Number: TXS0206 Hello,
According to the datasheet, the maximal clock frequency for the TXS0206 is 60MHz, while the maximal data rate is 60Mbps.
If I'm using the TXS0206 to interface to an SD card with a 4-bit bus width, as far as I understand, a…
Part Number: TXS0206-29 Other Parts Discussed in Thread: SN74AXC2T45 , SN74AXC4T774 Hello, I need an SD 3.0 compliant voltage level translator that can convert 3.3V signals from my processor to 1.8V signals for an SD card so that I can run UHS-I type cards…
Part Number: TXS0206 Is there good device of level shifter of SD card interface to support following condition in TI products ?
-3.3V and 1.8V voltage switching IC for SD card -0.4mm pitch BGA products are not acceptable ( Okay for QFN etc.) because our…
Part Number: TXS02612 Other Parts Discussed in Thread: TXS0206 Use TXS02612 all the way instead of TXS0206, or recommend high-speed SDIO, SD, EMMC level conversion chip in QFN package. Thank you!