Part Number: TXS02326A Tool/software: I want to run these two chips in parallel with 1 modem so I can utilize 4 outputs. Is there an EN function so that I can disable one of the IC's when I am multiplexing?
Part Number: TXS02326A Other Parts Discussed in Thread: TMUX1574 Tool/software: Hello,
My customer is looking for an analog switch IC with the following features;
Please recommend a suitable product among TI products.
Thank you.
JH
Hi Michael,
Michael Ikwuyum said: When you say I2C devices come up except this one, do you mean the I2C pins or the TXS device?
Ok, i mean by running, for example, the command "sudo i2cdetect -y -a 1" in the Raspberry Pi terminal. When you run this command…
Part Number: TXS02326A I'm trying to understand if my application will benefit in any way from the external clock. I understand that an external clock can offer higher stability, precision, and the ability to sync multiple devices. It looks like this…
Part Number: LSF0102-Q1 Other Parts Discussed in Thread: TXS0102 , TXS02326A , TXS02612 , TXB0102 , TXB0302 Tool/software: Hi. I am looking for voltage level shifter for MIPI RFFE application.
The product should operate up to 52MHz. (MIPI3.0 standard requires…
Part Number: TXS02326A Other Parts Discussed in Thread: BQ25895 Hello I 'm trying to start an I2C interface with the TXS02326A device but not yet successful. TXS02326A and bq25895 are connected to I2C bus on our board. The bq25895 device has the 0x6A…
Part Number: TXS02326A Hi
1. We do not use BSI input of TXS02326A.
Can we leave the BSI input open or we must it pull up or pull down if "BSI detection behavior" bit is 1 in register 0Eh?
2. IRQ is used to set the I2C address.
Is the IRQ signal…
Part Number: TXS02326A Other Parts Discussed in Thread: TXS4558 Hi Team,
My customer needs to know what difference between txs02326A and txs4558.
could you provide comparison table and introduction slide.
Thanks
Part Number: TXS02326A Hello
The "SETTING UP THE SIM INTERFACE" section of the TXS02326A datasheet describes how to start the SIM interface.
In item 3 of the sequence is writen: "The baseband SIM interface is set to a LOW state."
…
Part Number: TXS02326A Hi Sir,
Here are two Switching between SIM cards processes questions need your help.
1. How to put SIMx card interface into "clock stop" mode?
2. There are two scenarios when switching to SIM2 card are described on the…