Part Number: TXU0102-Q1 Tool/software: When a damping resistor (47Ω) is attached to the output (3.3V), when charging the input capacitance of the input device (e.g. 10pF), the following current flows instantaneously and exceeds the output current rating…
Part Number: TXU0102-Q1 Tool/software: Hi team,
How accurate is the internal pulldown resistance (5MΩ) ?
If that is a typical semiconductor, I think it is about ±20%.
Please share any information , even if it is not a specification.
Thanks…
Part Number: TXU0102-Q1 Tool/software: Hi team,
I would like to know the input level threshold and output voltage level when VCCA=3.3V and VCCB=1.8V.
Do you have data available?
Or if there is a way to approximate the calculation, please let me know…
Part Number: TXU0102 Other Parts Discussed in Thread: TCA9511A , LSF0102 , TCA9406 , PCA9306 , SN74LVC2G66 , TXS0102 , TCA9803 Hi team,
I'd like to know if VCCA and VCCB of TXU0102 can be same voltage and this device can be used as ON/OFF switch for I2C.…
Part Number: TXU0102 Hi Team,
If use TXU0102 as below connection, will the pull high or pull low resistor at end point will affect the B1/2Y voltage level?
For example: If B1Y have 70k ohm pull low resistor inside WIFI, is B1Y still 1.8V when A1 is 3…
Part Number: TXU0102 Hello,
A similar post regarding the -Q1 product, that the top side is 2PGT for it's topside. what is the top side for the non-automotive rated one TXU0102DCUR, the physical part that we have here at Digikey is 2PFT,
Part Number: TXU0102-Q1 Hi,
I don't find the specifical marking for this component (TXU0102QDCURQ1).
Could you help me, what is the marking please ?
thanks
Part Number: TXU0102 Other Parts Discussed in Thread: TXU0202 , Hi support team.
If you check the datasheet, you will see that there is a part where the B port is expressed as an input. This device was capable of level conversion only in a fixed direction…
Part Number: TXU0102 Hi support team.
Is there any material that roughly explains the internal input/output circuit?
We received a request from my customer.
We would appreciate your cooperation.
Best regards,
Higa
Part Number: TXU0102 Other Parts Discussed in Thread: SN74AXC4T774 , , TXB0104 , TXU0304 , TXU0104 , TXU0204 Hey team,
I am in search of a SPI level shifter IC that would translate 3.0V to 1.8V. It needs to be able to handle SPI speeds up to potentially 12MHz…