Part Number: TXU0104 Other Parts Discussed in Thread: LSF0204 Good Morning.
I'm using TXU0104 component to translate signals from +1,8V to +3,3V and the inverse, from +3,3V to +1,8V.
In the datasheet, I have seen that 50Mbps minimum data rate is indicated…
Part Number: TXU0104 Other Parts Discussed in Thread: TXB0604 , SN74AXC4T774 Hi team,
Customer is evaluating TXU0104 in their wearable application.
They find there is the power consumption data under normal condition.
They also care alot about the…
Part Number: TXU0104 Hello, We are planning to use the TXU0104PWR in one of our projects, where four flow sensors are connected to Port A of the translator, and Port B is connected to the ESP32. We are translating the 5 V sensor signals to 3.3 V logic…
Part Number: TXU0104 Hi Team,
We are interfacing the TXU0104PWR with an encoder that operates at 5 V and is compatible with CMOS and TTL logic levels. The translated signals will be connected to the FPGA.
Could you please review the schematic and…
Part Number: TXU0104 Hi team,
What is positive going input threshold voltage when Vcc is 5V? Datasheet describes about VCC = 4.5V and 5.5V.
Best regards, Goto
Part Number: TXU0104 TI support,
Could you please clarify if the test conditions for VOL and VOH specs refer to steady state current or peak current during a switching event?
Thanks!
Part Number: TXU0104-Q1 Tool/software: Hello Team, We are using the IC TXU0104-Q1 to level shift SPI signals of 3.3V to 5V logic.
The slave out pin is not used in the system.
The 3.3V side is connected to the VCCA and 5V is connected to VCCB.…
Part Number: TXU0104 Tool/software: What's the typical/max VCCA current for the following specific conditions:
VCCA = 3.3V
inputs are logic HIGH (3.3V)
VCCB is floating
Thank you!
Part Number: TXU0104 Other Parts Discussed in Thread: TLV9034 , SN74AXC4T245 Hello,
We would like to use the TXU0104 to interface with an IC with 1V logic levels (IC provides 1V input to TXU0104 and level shifts it to 3.3V). The positive-going threshold…