Part Number: TXB0104 Other Parts Discussed in Thread: TXU0304 , TXU0202 Hello.
I want to use TXB0104 AS SPI BUS LEVEL SHIFTING/TRANSLATOR 5V TO 3.3V.
I also will need RX TX (UART COMMUNICATION) TRANSLATOR 5V TO 3.3V IN THE SAME PCB.
I want to use…
Part Number: TXS0104E Other Parts Discussed in Thread: TXU0202 Hello,
We were using the TXS0104E with a high impedance input.
The device seems to be pulling down on the input when shutoff. (more details below)
Your feedback to us at the time was…
Part Number: LSF0204 Other Parts Discussed in Thread: TXU0202 , Hello,
we need to use this transceiver as Push-pull.
how this can be used?
Regards,
Sudharshana
Part Number: SN74LVC8T245 Other Parts Discussed in Thread: TXU0204 , TXU0202 Hi Team,
My customer has some queries regarding the SN74LVC8T245. Can you please help answer the below?
• Clarify whether the above mentioned part supports for UART Communication…
Part Number: TXB0302 Other Parts Discussed in Thread: TXU0202
Hi
We are using TXB0302DQMR in our design. Following is our implementation
Since INTR signal( connected to pin 2) is an open drain signal we are facing issue.The signal is not toggling…
Part Number: TXU0304 Other Parts Discussed in Thread: LSF0108 , TXV0108 , TXV0106 , TXU0104 , TXU0102 , TXU0202 , TXS0108E Tool/software: Hi,
I am looking for a SPI level shifter however I need one which can handle multiple devices.
Ideally would…
Part Number: TXB0102 Other Parts Discussed in Thread: TXU0202 Tool/software: I recently added TXB0102 to make the UART level translation from an MCU at +3.3 V (PIC18F47J13) to send AT Commands to a Modem at +1.8 V (Quectel BG600L-M3), however, in my design…
Part Number: TXS0102 Other Parts Discussed in Thread: TXU0202 , Hi, Support Team
as below schematic is workable?
Sould I OE pin connect to MCU GPIO and pull down to GND?
also i confused about Transceiver and level shift is mean same parts? or…
Part Number: LSF0102 Other Parts Discussed in Thread: LSF0002 , TXU0202 , TCA9800 Tool/software: Dear TI experts,
My customer is looking for LSF0102 for a level translation of UART and I2C.
They will connect A side to MCU interface. The problem is…