Part Number: TXV0106-Q1 Tool/software: Hello,
I'm planning to use the TXV0106-Q1 on a platform where I do not need the OEb pin and the default VCC Isolation feature is sufficient for my needs to keep the IO high-Z during power up. I was planning to…
Part Number: TXV0106-Q1 Tool/software: Hi Teams:
Due to the limited PCB layout space, we have not placed termination resistors at the signal source end, and we also cannot reduce the driving capability of the output, which affects the signal's edge time…
Part Number: TXV0106 Other Parts Discussed in Thread: TXV0108 Tool/software: Hello.
As written in the title, I would like to request a review because it appears to be an error in the data sheet. (descriptions that has a fixed direction but is treated…
Part Number: TXV0106-Q1 Tool/software: Hello team:
I have some questions about the output channel-to-channel skew and duty cycle variation described in the datasheet:
1. How are these two parameters measured, and what methods are used to obtain the values…
Part Number: TXV0106-Q1 Other Parts Discussed in Thread: TXV0106 Hi Team,
We are designing TXV0106 in RGMII and want to double check if this device can support 150mm trace length.
We know there are some parameter will impact the result, but in general…
Part Number: TXV0106-Q1 Hello, I wanted to confirm the max data rate for this part? In one location you say max data rate of up to 500Mbps for 1.65 to 3.6V. In another you say 250Mbps/channel for RGMII 2.0.
Can you please confirm this port supports 250Mbps…
Part Number: TXV0106-Q1 Other Parts Discussed in Thread: SN74AVC2T45-Q1 , Please provide IBIS model and project details as follows
Device name of the model you are requesting :
SN74AVC2T45-Q1
TXV0106-Q1
Project details :
For simulating a 100Mbps application…
Part Number: SN74AXC4T774-Q1 Other Parts Discussed in Thread: TXV0106-Q1 , SN74AVC4T774-Q1 Tool/software: Though the datasheet claims speed of 310Mbps while converting 1.8V to 3.3 V signal, the measured data comes no where close to this. What could be…
Part Number: SN74AXC4T774-Q1 Other Parts Discussed in Thread: TXV0106-Q1 Tool/software: Hi team,
My customer is using this device as 1.8V to 3.3V level shifter for TDM signal. It is sensitive for the propagation delay time. The delay time will have impact…