Part Number: TXV0108-Q1 Hi team,
Could you please advise the minimum propagation delay level shifter for my use case below?
I/F : SPI
data rate : 25MHz
I found TXV0108-Q1. Is this the right device?
Since slave device has large propagation delay variation…
Part Number: TXS0108E-Q1 Other Parts Discussed in Thread: TXV0108-Q1 Tool/software: Hi Team,
In our design, we are going to using TXS0108E-Q1 IC for RMII interface (Like as TX and RX connection are connecting in only one Level translator). Can we use…
Part Number: TXS0108E-Q1 Other Parts Discussed in Thread: TXV0108-Q1 , LSF0108-Q1 , LSF0108 , TXS0108E Tool/software: Hi Team,
In our design, we are going to use TXS0108E-Q1 IC for MII Mode (Speed: 100Mbps) interface (TX and RX pin connection are connecting…
Other Parts Discussed in Thread: TXV0108-Q1 FAQ: Logic and Voltage Translation > Fixed DIR / DIR CNTRL Level-Shifters >> Current FAQ
Data rate depends on the system designers tolerance for various parameters such as VOL / VOH levels, duty cycle distortion…
Part Number: TXV0106 Other Parts Discussed in Thread: TXV0108-Q1
Hello Team,
shouldn't Vcca and Vccb be switched for the lower part as this is a unidirectional level shifter?
Also Vout(min) should be corrected to 1.14V in the search parameters, right…
Part Number: SN74LVC244A Other Parts Discussed in Thread: TXV0108-Q1 Hi,
RnD currently used SN74LVC244A for the signal 50MHz. The output signal is distortion.
Is there solution for high speed (tpd < 5.9ns)?
Thanks and Best regards,
Part Number: SN74AXC4T245 Other Parts Discussed in Thread: TXV0108-Q1 , TXV0106-Q1 Hi Team,
We are using the SN74AXC4T245PWR IC for level translation. In the datasheet, it is given that the data rate supported whea.n translating from 1.8V to 3.3V is up…
Hi All,
Please see the new TXV level-shifter family (TXV0106-Q1 / TXV0108-Q1) supporting high-bandwidth timing-margin sensitive interfaces such as RGMII.
For more information, see Enabling high performance interface translation | Video | TI.com , thanks…