Part Number: UC2825A-Q1 Other Parts Discussed in Thread: UC2825 , UCC28951 , UCC39002 Hi,
I am designing a 3-phase interleaved buck converter to convert an 800 VDC input to a 400 VDC output.
To validate the semiconductors and the inductor of a single…
Part Number: UC2825A-EP The datasheet for UC2825-EP specifies the supply current at a specific operating point. Does the supply current change based on operating frequency? Does the supply current assume a load or is this only specific to the operation…
Part Number: UC2825A Other Parts Discussed in Thread: LM5035 Tool/software: hi expert , i want to use uc2825a for a full bridge design, but this device has only two driver output . any ideas of how to drive synchronous rectifier
MOSFET using OUTA and…
Part Number: UC2825A-EP
Hi
We would appreciate clarification on the implementation and capabilities of the VREF pin on the UC2825A-EP IC:
What is the internal architecture of the VREF output? Is it generated using an internal LDO/regulator or…
Part Number: UC2825A-EP Hi
For oscillator frequency determination, datasheet mentions that max. duty cycle should not be less than 70%. Is this the max duty cycle for each output (OUTA & OUTB)? I plan to use this IC for an application which where both…
Part Number: UC2825A-EP Tool/software: Hello,
The UC2825A-EP TI webpage shows as device having a 50% max duty cycle. However, the datasheet shows 85% duty cycle max. Which is right??
Part Number: UC2825A-EP Other Parts Discussed in Thread: UC2825A Hi,
Is there any clock IC that can generate 100KHz of 1us or less pulse width to sync multiple UC2825A controllers?