Part Number: UCC27517A-Q1 Tool/software: The below total component FIT rate should be sum of die FIT and package FIT. Could you please help correct it?
Part Number: UCC27517A-Q1 Other Parts Discussed in Thread: UCC27517A Tool/software: Dear Rubas,
As you know we are using TI gate driver ucc27517A-Q1 ic with our PFC+LLC controller to drive PFC mosfets . PFC out put is 390V - 2.99A.
In previous mail we…
Part Number: UCC27517A-Q1 Other Parts Discussed in Thread: UCC27517A , UCC28180 , UCC25660 We are using gate driver ic UCC27517A-Q1 with our (pfc + llc) controller, our pfc controller output is 390v- 2.99a.
we are facing some problem, in gate driver ic…
Part Number: UCC27517A-Q1 Hi Dear
I have been informed of the following question from customer.
Has UCC27517A-Q1 already been qualified for AEC-Q006 ?
If not yet, would you please tell me when it will be?
In hybrid electric vehicles/electric vehicles (HEV/EV), the engine is not used to run the heating and cooling system like it is done in the internal combustion engine (ICE) vehicles. To replace this function, two key systems are being used: a BLDC motor…
Part Number: SN74AHCT1G126-Q1 Other Parts Discussed in Thread: UCC27517A-Q1 , CD40109B-Q1 Hi team,
I have a customer that wants to use the SN74AHCT1G126-Q1 for their design to move 3.3V logic to 6.5V, however the part says the max is 7.0V and they feel…
Part Number: UCC27517A-Q1 Dear, Sir.
My customer is considering to apply UCC27517A-Q1 for their automotive system.
Now, they are cheking the capability against reverse battery.
Before, they faced a trouble on other supplier's product such as;
…
Part Number: UCC27517A-Q1 Hi AC/DC Team
I want to design RC Filter circuit in IN+ input line because PWM noise as a blow
input spec: 12V, 500Khz, Vp-p: 0 ~ 5V
Do you recommend R1 value range and C18 value?
Thanks
Best Regards
Gerald
Part Number: SN74AHCT1G125-Q1 Other Parts Discussed in Thread: UCC27517A-Q1 Hello,
I am using the buffer SN74AHCT1G125-Q1 for driving MOSFET with Vcc=5V. Gate resistance of 10 Ω was added, so gate current will be 500mA (5V/10Ω). Whether this buffer…
Part Number: UCC27517A-Q1 Other Parts Discussed in Thread: UCC27517 Hi All,
What's the input parasitic capacitor value for UCC27517A-Q1 IN+/- pin? thanks.
Best Regards
Charles Zhang