Part Number: UCC27527 Hello
The Heat dissipating pad on the underside of WSON
package whether it is electrically connected inside.
Specifically if I do not use it , to say, connect to GND,
would there be any performace issue?
My heat dissipation…
Part Number: UCC27527
Hello
I plan to use UCC27527 in my Pre Driver stage for IGBT Drivers
where Dead Bank & Interlock and Short Pulse Suppression Ckts shall be built-in
I have the following Q's:
1. Is it also available in SOIC package?…
Part Number: UCC27527
Hello
I've two Q's reg the above.
1. Data Sheet mentions,
" The maximum voltage on the Input and Enable pins is not restricted by the voltage on the VDD pin. "
Does it mean that INA or INB can exceed the Vdd supply?
2…
Hi Mamdou
If not asking for too much ; can you please also evaluate
CD4050 ( Singly ) ; CD4049 ( Dual Cascaded ) and CD40106 ( Dual Cascaded )
against UCC27527 for this application ?
Their larger Footprint initially discouraged us from considering…
Part Number: UCC27527 Other Parts Discussed in Thread: LM5111 , Team,
We currently use the LM5111-1MY to drive a DUAL MOSFET that in turn drives a transformer. While working through a legacy design that uses the LM5111 I have discovered we are actually…
Part Number: CD4050B Other Parts Discussed in Thread: TLV1811 , TLV7211 , UCC27527
Hi Clemens
Thanks for your prompt support in the past.
I've a few supplementary Q's, answers to which I could not gather from the Data Sheets.
Pl be good enough…
Part Number: UCC27528 Other Parts Discussed in Thread: UCC27527 , UCC27624 , UCC27614 Hi,
Good Day.
Would you recommend a gate driver for the UCC27527/8 (it is also a gate driver) for switching application.
Both devices are going to drive the STL3N10F7…
Part Number: CD4050B Other Parts Discussed in Thread: UCC27527 , CD40106B
Hi
I had asked a Q reg UCC27527 Input characteristics .
This is a related Q
We want to create a Short Pulse Suppression Ckt for our 0-15 V Signals from the DSP
Typical…