Part Number: UCC33020-Q1 Other Parts Discussed in Thread: UCC33010 Tool/software: Hi, I'm designing a fail-safe circuit that operates at 3.3V input and output. The output should be enabled using the pwm format enable signal; otherwise, it should be disabled…
Part Number: UCC33020-Q1 Other Parts Discussed in Thread: UCC33010-Q1 Tool/software: Interested in UCC33010-Q1 , it is an active item? Quotation tool show it is invalid MPN
Part Number: UCC33020-Q1 Tool/software: We are evaluating the UCC33020-Q1 isolated DC-DC power module for our new BMS design, comparing it with our previous design, which used the PDSE1-S12-S5-M-TR module. In our current design, we have a Y capacitor…
Part Number: UCC33020-Q1 Other Parts Discussed in Thread: UCC33420-Q1 , UCC14241-Q1 Tool/software: In order to have a higher power output, is it OK to connect multiple UCC33020-Q1's output VCC in parallel directly? Or, do they have to go through a diode…
Part Number: UCC33020-Q1 Tool/software: Hi expert,
Do we have power module which operating current with no load less than 1mA (UCC33020-Q1 is 7mA as below)? My customer need a lower power devices.
Best Regards,
Ryker
Part Number: UCC33020-Q1
Tool/software:
Hi expert,
Can customer use a 10nF capacitor in COUT1 and CIN1? They haven't 15nF capacitor.
Best Regards,
Ryker
Part Number: UCC33020-Q1 Tool/software: Two weeks ago I found the UCC33020-Q1 to be a potential solution for an isolation problem that I was finding in my design. At this time it was 500 parts as TI inventory. Now I have finished the prototype project…
Part Number: UCC33420 Other Parts Discussed in Thread: , UCC33410 , UCC33410-Q1 , UCC33421-Q1 , UCC33411-Q1 , UCC33020 , UCC33020-Q1 Tool/software: Hi,
We are planning to use below new products from TI. We wanted to confirm availability of these parts…
Part Number: UCC33420-Q1 Other Parts Discussed in Thread: UCC33020-Q1 Tool/software: Hello TI team,
We are currently developing an ECU module, where the hardware needs a 5V to 5V DC DC auto grade isolated converter. We have identified two parts of TI…
Part Number: TCAN1145-Q1 Other Parts Discussed in Thread: ISO7741-Q1 , UCC33020-Q1 , ISO7742-Q1 , ISO7741 , ISO7041-Q1 Tool/software: Hi expert,
My customer (CosMX) is looking for a low power Isolated CAN solution, they need to achieve <1mA quiescent…