Part Number: UCD3138128A Tool/software: Hi,
When I boot up my Fusion Digital Power Designer, I am unable to bring up the Memory Debugger when the device is in PROGRAM Mode.
Here is my screen... Thank you for any help in this matter.
Part Number: UCD3138128A Other Parts Discussed in Thread: UCD3138 , UCC29002 , UCD3138128 , TIDA-00653 Tool/software: Hello everyone
I am also interested in using the UCD3138 IC to design an isolated DC-DC boost converter with the following main characteristics…
Part Number: UCD3138128A Hi,
I need to know the total supply current for UCD3138128APFCR.
Here, what current I've to consider?
Please help me with this.
Thanks
Part Number: UCD3138128A Other Parts Discussed in Thread: UCD3138128 , , UCD3138A64 , UCD3138A64OEVM-662 Tool/software: We are having trouble enabling the SPI signal TDO and TDI as GPIO outputs.
Is there other discussions about this I could examine…
Part Number: UCD3138128A Other Parts Discussed in Thread: UCD3138128 , Hello TI friends,
Now we want to use UCD3138128A for FB-LLC DC/DC covert design, the another is boost. We refered demo uses UCD3138128.
So I want to know what's the difference…
Part Number: UCD3138128A Hello,
In a DC/DC full-bridge power supply topoly, what would be the maximum frequency acheivable for a current mode control ?
If Current Sense signal at primary is at 1MHz or 2MHz cabled to EA2+/- inputs, is a peak current…
Part Number: UCD3138128A hello,
Do you have information to start a development with these requirements?
Is it possible using UCD3138128A part?
Vin : 35-55V
Vout : from 75V to 500V
P = max 750W
thanks in advance for your help.
Lauren…
Part Number: UCD3138128A Other Parts Discussed in Thread: UCD3138064A , UCD3138OL64EVM-031 When use XDS510 usb PLUS connect UCD3138128A by JTAG port, it can't be connected.
UCD3138128A is put in socket of UCD3138A640EVM-662 socket.
I use another UCD3138OL64EVM…
Part Number: UCD3138128A Other Parts Discussed in Thread: UCD3138 , The impact of previous channel sampling on the current channel and its relationship with high and low temperatures; Why is low temperature less affected when the previous channel signal…
Part Number: UCD3138128 Other Parts Discussed in Thread: , UCD3138 Hi Team,
My customer change the UCD3138128A to UCD3138128.
They see his board will reset when they test the surge CM2.0KV from system side through in.
and they try to turn the reset…