Part Number: UCD9244 Other Parts Discussed in Thread: UCD74120 , UCD7242 , TMS320C6678 , Team,
My customer is seeing this intermittent issue:
I have a board with two TMS320C6678 DSPs. They are being powered by a UCD9244 along with UCD74120 for CVDD and a…
Hi Johnson,
We are using TCI6638K2K part. Here the EVM has two CVDD supply (UCD9244 + UCD74120). As per TCI6638K2K datasheet, only for the DSP core variable and fixed supplies are used. For ARM core only fixed supplies are used.
As per the estimation 20A…
Part Number: CSD95377Q4M Other Parts Discussed in Thread: UCD9224E , UCD9246E , UCD9248E , UCD9222 , UCD9244 , UCD74120 , UCD9246 , UCD74111 Is CSD95377 easily compatible with UCD924x digital controllers?
It looks like they would match up well, I believe UCD924x…
Part Number: UCD9246 Other Parts Discussed in Thread: LM57 , LM94022 , UCD74120 We would like to use the LM57-10 to measure the board temperature of our UCD9246 based design. This will be fed directly into the "TEMPERATURE" pin, w/o a mux.
Fusion…
Part Number: FUSION_DIGITAL_POWER_DESIGNER Hello. I have designed a power solutions with two UCD9248 (with descrete drivers UCD74120) working as a system. I would like to describe issues that I have faced.
1. The first system I started as offline project…
Part Number: UCD9248 Other Parts Discussed in Thread: UCD74120 , UCD7242 , UCD7232 hi,
i am new to power section design .
1. does any EVM boards available for programming UCD9248?
2. whether TIs USB Interface Adapter EVM can be used ?if possible please…
Joe,
The K2H EVM contains 2 different UCD9244 devices where each controls 4 separate power conversion devices. The first 2 channels of U16 control the AVS supply. These come into the VID1 and VID2 inputs but the VID2 inputs are no longer used. At one…
Part Number: 66AK2H12 Other Parts Discussed in Thread: UCD74120 , UCD9244
Team, I got the feedback from an EVM's user that the Smartreflex might not be working accordingly on the K2H EVM. I have seen already the below posts that explains why 2 Smartreflex…
Hi Bill,
In EVMK2H's schematics, one UCD9244's channel 1A outputs one PWM signal that is Farm0_PWM-1A to controller two UCD74120s that are combined together to supply for CVDD. The signal Farm0_PWM-2A is not used really.
And this UCD9244's…