Part Number: UCD90320UEVM Other Parts Discussed in Thread: UCD90320
We are currently evaluating the UCD90320 and would like to ask a question regarding its power-down (re-sequence) behavior when a fault is detected.
When a fault is detected during…
Part Number: UCD90320U The UCD90320U can log a System Watchdog Timeout Fault in its internal flash only the FIRST time it appears. To register another one, the device must be reset, otherwise all the System Watchdog Timeout Faults will not be logged.…
Part Number: UCD90320 Hello,
I have created a example project on the UCD90320UEVM dev kit with the SECURITY option OFF.
I have exported 2 .csv files with the "Data Flash Script" generation tab that I use with the Script Runner Tool from Ti.
One…
Part Number: UCD90320U Other Parts Discussed in Thread: UCD90320 Hello,
I have detected an issue with the feature "Ignore Input during delay" of a LGPO.
I configure LGPO #1 = NOT ( GPI #2) with a 50 ms delay.
Delay when asserted = ON
Delay when…
Part Number: UCD90320 Hello,
I have created a example project on the UCD90320UEVM dev kit with the SECURITY option ON with the following password : 123456 .
I have exported a .csv file with the "Data Flash Script" generation tab that I use with the…