Part Number: UCD9081EVM Other Parts Discussed in Thread: UCD9081 Hello TI Support Team,
I am working with the UCD9081 power sequencer and need clarification regarding the usage of its GPIO/GPO pins.
I would like to use GPO1 to GPO4 to drive pulses…
Part Number: UCD9081EVM Other Parts Discussed in Thread: UCD9081 Tool/software: Hi,
I try to read the UCD9081 Device ID of 0x55 from register 0x27, but it reports 0x00. I use a custom USBC to I2C bridge board for this purpose.
Br,
Mozhdeh
Part Number: UCD9081EVM Other Parts Discussed in Thread: UCD9081 Hello,
My customer is using the UCD9081EVM and trying to communicate with it using a general USB-I2C device.
They have J17-J20 (ADDRx pins) all set high so the address is 0x6F. They…
Part Number: UCD9081EVM Other Parts Discussed in Thread: UCD9081 , Hello,
As with others the hardware is not detected, what I have triued thus far:
Update the firmware on the TI USB interface adaptor to 1.0.11
Set the bus speed to 100kHz
Disabled…
Part Number: UCD9081EVM Other Parts Discussed in Thread: UCD9081 Please tell me did the UCD9081 EVM GUI program with the USB Interface Adapter can work under Win98?
I could not make the win98 recognize the USB Interface adaptor
Thanks
Uri…
Part Number: UCD9081EVM Other Parts Discussed in Thread: UCD9081 I just received my UCD9081 EVL kit. I have TI fusion designer installed 7.3.1 as well as the UCD EVAL GUI.
The eval kit is powered up , all bus rail voltage LED's are lit. I have a green…
is this a new USB-to-GPIO dongle? maybe unplug and plug the usb cable or reboot your PC.
you can install the Fusion digital power designer from www.ti.com and refer section 2.2 of www.ti.com/.../slvub51.pdf to download the FW.
Regards
Yihe
Hi Yihe,
I tried to use the low level I2C tool on the UCD9081EVM. I connected the scope to the I2C test points on the EVM and i see I2C signals!
When using the EVM GUI I'm not seeing signals. Not when trying to open the GUI and not when trying to…