Part Number: BQ25703A Hello, I was reading the datesheet of BQ25793A . I am looking for implementation of this IC to charge a 2-S lipo battery
But my doubt is if I could use this IC without MCU, I mean I would like to use only the BQ2579A with an USB-C…
Part Number: DP83TD510E-EVM Other Parts Discussed in Thread: USB-2-MDIO I'm trying to power DP83TD510 and connected DP83822 with USB from PC or USB charger. I installed J9 jumper (USB power), and left all other jumpers as default (EXT pins left disconnected…
Part Number: USB-2-MDIO Hi,
I have connected the MSP430F5 to a DP83TC812 MDIO interface, using the USB-2-MDIO application, and I have seen that the response from reading a register is rotated.
See below: instead of default value 2100, the value is 4201…
Dharrvin
You can use either 100nF or 220nF for SSTX1 and SSTX2.
Does the FLIP pin change its voltage for the normal and flip Type-C orientation? You should see 0V on FLIP pin for the normal orientation and 3.3V for the flip orientation.
For USB3.2 Gen2…
Hi Varun,
Using the .prj file you provided does the following:
The EVM negotiates power from the two USB-C ports. If only a NoteBook (is this NB in your description?) is connected to Port A, then SYS is powered with 5V. If Port B is then connected to…
Part Number: USB-2-MDIO HI,Friends,
I operate USB-2-MDIO and MSP430G2 LaunchPad to configure DP83848KSQ's registers via MDC/MDIO interface,
MSP430G2 LaunchPad pin configurations are as follows: • MDIO (EVM) Connect to P1.5 (LaunchPad) • MDC…
Part Number: CC2540EMK-USB Other Parts Discussed in Thread: CC2540 , CC2642R I want to bridge CC2540EMK to Wireshark. I installed packet sniffer2 for that. But I didn't find the corresponding driver for CC2540EMK. I am using Windows 10.
I found in this…
Part Number: TPS65981 Other Parts Discussed in Thread: TPS65987 Hi we have the 69581 running as a DRP. We have a specific application where our customer is unable to connect the CC signals and as such unable to do a PD power negotiation.
We can change…
Part Number: DP83TD510E Other Parts Discussed in Thread: USB-2-MDIO , MSP430F5529
Team,
Seems like the G2 LP recommended is not available anymore. MSP-EXP430G2ET seems to have replaced the MSP-EXP430G2 listed in the USB-2-MDIO UG. -Can any MSP430 LP card…