Part Number: USB-PD-CHG-EVM-01 Other Parts Discussed in Thread: TPS25750 , BQ25798 , BQ25792 , TPS25751 Tool/software: Hello, I just purchased the USB-PD-CHG-EVM-01 to charge a 3S battery (using sink capability only) using both "USBCPD Application Customization…
Part Number: TUSB8041 Other Parts Discussed in Thread: HD3SS3220 Tool/software: Can we use a USB Type-C connector as the input USB interface for the TUSB8041? If so, are there any specific considerations or additional components required for this configuration…
Part Number: PMP40001 Other Parts Discussed in Thread: BQ25731 , TPS25751 , , LM5175 , PMP41062 , BQ25756E , PMP41031 , TPS25750 Tool/software: I'm designing a product similar to PMP40001, and am planning on using the TPS25751 for USB-PD interface (dual role…
Part Number: TPS25751 Other Parts Discussed in Thread: TPS65988DK
Hi,
Im looking for a USB type C PD controller IC.
We need 3 usb type C ports in our design. One port should support both power in (140W) and power out (65W) and the other 2 ports should…
Part Number: USB-PD-CHG-EVM-01 Hi Team,
Currently my customer is having USB-PD-CHG-EVM-01 evaluation board. with below tools:
1.usb2 any
2.aardvark programmer
They tried to download aardvark programmer from total phase but they were unable to flash it…
Hello Irving,
I am having the same connecting issues with a USB C cable from UGREEN, but I can connect with another one.
Eitherway, the HDMI is not working and I wanted to see if it had something to do with the USB issue.
If you could also send me the…
Thank you for the clarification. In that case, the TPS65988DK would be the best device. This is a dual port USB-PD controller capable of supporting DisplayPort and a 100W USB-PD contract.
Part Number: HD3SS3220 Tool/software: Hi Team,
(1) Does HD3SS3220 NHR have USB Type-C IF specifications?
(2) HD3SS3220IRNHR needs to be certified by USB Type-C IF. Is there a relevant design guide or reference design that can be provided?
Part Number: BQ25672 Tool/software: Hi TI Team,
we are currently looking for a Battery charger IC with MPPT and Solar Support. Idealy with dual input selector for USB-C and Solar.
I attached a screenshot of the typical application diagram with two inputs…
Part Number: USB-PD-CHG-EVM-01 Other Parts Discussed in Thread: BQ25798 , BQSTUDIO Hi,
I am currently testing a Powerbank USB-PD solution and I use the USB-PD-CHG-EVM-01 demo board seems to match my need. I would like to program the BQ25798 registers myself…