Nikhil D,
Using google I found someone who had the exact same problem with an NXP system. It is caused by a change in gstreamer.
I have finally got 4 cameras to work just as I did with kernel 4.4.45. The modifications I had to make to the isl79987…
Part Number: TMS320C6678 Other Parts Discussed in Thread: SYSBIOS
Tool/software:
[ CCS Version: 5.5.0.00077 ]
[Custom Board with NO IBL.]
[RTOS, SYS/BIOS]
Hi,
I'm trying to boot a large objet file from SPI-NOR Flash, so it needs to INIT…
Dear All,
We have beagle bone black prototyped custom board, where we replaced the existing DDR with "MT41K128M16JT-125M:K DDR3". We are usingDDR3L-1600 Speed Bins. We are trying to update the timing parameters in DDR3 timing configuration tool spread…
Part Number: TPS40057 Hi,
I am considering a sink circuit using TPS40057. Operating condition = input 12 V ± 10%, output 2.5 V, output current -1 A (sink only) Used as power supply for LCD Vcom. The circuit constants are determined based on the calculation…
Sebastian ,
Can you please provide input and inductor current waveform when the output goes low ?
Further here are few comments on your layout and Schematic :
1. I dont see any decoupling cap on Vin pin of the device . Please place a cap as close…
Hello, I keep getting "file type is not allowed" for the .xlsm extension. I have renamed it to .xls for the upload. LM5146-LV5144_quickstart_calculator_revB1_09-05-2024.xls Also attached are the SW & low side gate waveforms (with the original PCB configuration…
console=ttyO1,115200n8 consoleblank=0 vram=50M root=/dev/mmcblk0p2 ro rootfstype=ext4 rootwait
the defconfig is minor changes on top of the tisdk_am335x_defconfig.
1004.defconfig.txt
the start-up script is updated a bit in our case, so, inittab…
Part Number: LM5185 Tool/software: Hi TI team,
I have created the schematic 50W Iow cost Isolation design using LM5185 with the requirements as below:
- Input: 36-75V
- Output: 12V4.2A
I kindly request you to review the attached updated my schematic…