Part Number: WILINK-HW-DESIGN-REVIEW Hi Support Forum,
Apologies for the pre-selection of categories, but I couldn't find a way to mark this as a "Your web server is reporting something that is no longer working".
This is about the following repository…
Part Number: LM51772 Email
Technical Support Request – LM51772 Output Voltage Configuration and Load IssueTechnical Support Request – LM51772 Output Voltage Configuration and Load Issue
Hi Ti,
We have developed a power supply design based on the…
Part Number: LM7480-Q1 Hi ,
Could you please validate the attached schematic?
Below are the design requirements and operational parameters for this application:
Power Inputs & ORing Configuration
U1 (LM74700D): Connected to a +24V input…
Part Number: LM7480-Q1 Other Parts Discussed in Thread: INA302 Hi ,
Could you please validate the attached schematic?
Below are the design requirements and operational parameters for this application:
Power Inputs & ORing Configuration
U1…
Part Number: TPS25985
Hi Team,
Please help to review the design schematics and layout.
The design requirements are:
Vin = 12 V,
22A for OC protection with a time constant of ~100ms
32A for SCP with a time constant of ~10us
Thanks for your…
Hi Feng,
We have made changes to the design of LM5122 based on your suggestions. Can you help review the schematic diagram?The input is 12V and the output is 19V/10A.
LM5122_SCH.pdf
Thanks,
Kind Regards
Part Number: CSD23285F5 Can you please review my MOSFET Switch Design Review in PM? I can PM the design and explanation so the expert can check whether it will work accordingly.
Part Number: SN74AXC1T45 Can you review my level shifter design in PM? I can PM the design and explanation so the expert can check whether it will work accordingly.