Part Number: WL1801 I'm using a SOM imx6 from Variscite including a WL18MODGI component.
When Linux (Yocto Scarthgap) is bootong, I have these message:
wlcore : wl18xx HW : 183x or 180x, PG 2.2 (ROM 0x11)
…
wlcore: PHY firmware version: Rev 8…
Part Number: WL1801 Tool/software: We are using Wi-Fi module of Murata having TI chip set WL 1801 in one of our old product. During the EMI/EMC tests we sometimes face issue of communication break. When we debug it we found that module is powered up but…
Part Number: WL1801 Other Parts Discussed in Thread: WL1831 Tool/software: Hi AM62SIP and WL1801 Champ !
My customer only plans to use 2.4ghz wifi.and we plan to use a single chip of WL1801 or WL1831 on the AM62SIP based board.
Will there be any…
Part Number: AM623 Other Parts Discussed in Thread: WL1801MOD , WL1837 , WL1801 , WL1271 , WL1835MOD Tool/software: I have a custom board based on the AM6231 which has a WL1801MOD chip on it. The board has no ethernet. We are running with Linux, I see…
Part Number: WL1801 This document from TI states that the maximum number of nodes on an 802.11s mesh network is 32 when using the HWMP routing protocol. Is this limitation still present when using an external routing solution such as B.A.T.M.A.N.?
Part Number: WL1801 HI, I have been having trouble getting the RTTT windows tool up and running with a WL1801 on our test board. I can connect and see the below:
But when I try to load the .bin and .ini, it gets ~75% through, seems to poll the…
Part Number: WL1801MOD Other Parts Discussed in Thread: WL1801 , Tool/software: I have tried to get my WL1801 interface to acquire an IPV4 address using HOSTAPD, WPA-SUPPLICANT, and NETWORK-MANAGER. None of them work, I get no response at all from the…
Part Number: WL1801MOD Other Parts Discussed in Thread: WL1801 I am bricking WL1801 modules. They do not respond to sdio initialization, so the linux driver does not load. Is there a way to recover these?
Part Number: WL1801 Hi
Our product has WL1801 working with Wilink8 software.
Just 2.4GHz WLAN works on it. 5GHz WLAN and Bluetooth is not needed.
WL1801 silicon is not available right now but we have some stock of WL1803 chips.
Then now we are…
Part Number: WL1801MOD Other Parts Discussed in Thread: WL1801 , WL1835MODCOM8B What is the required EVM for evaluating WL1801 together with AM437x Sitara device?
WL1835MODCOM8B together with AM437x EVM?
Regards, Frank