Part Number: WL1801 Other Parts Discussed in Thread: WL1831 Tool/software: Hi AM62SIP and WL1801 Champ !
My customer only plans to use 2.4ghz wifi.and we plan to use a single chip of WL1801 or WL1831 on the AM62SIP based board.
Will there be any problem…
Part Number: WL1831 Other Parts Discussed in Thread: WL1801 , , Hello, we need assistance in identifying the TI part number from image below. From the datasheet we know that WL18x1 chips are produced in DSBGA 130 balls package, but chip as shown on image…
Hi Lokesh,
We don't see an explanation for the deauthentication messages in the firmware or sniffer logs. Could you please provide debug logs for hostapd? This is done with attaching "-d" when launching hostapd binary.
Hello,
KOUSIK K said: After the enable line is applied high, the WL_IRQ is changed to drive logic '0' " : This is not happening in our case. WLAN_IRQ is held high always after power-up.
As I mentioned before, this is the problem. I would like…
Part Number: TM4C123GH6PM Other Parts Discussed in Thread: WL1831 , WL18XXCOM82SDMMC , WL1831MOD
I would like to inquire about the process of connecting the TM4C123GH6PM microcontroller and the WL1831 Wi-Fi and Bluetooth transceiver. Specifically…
Part Number: WL1831 Hello,
I'm currently using a module based on WL1831 with TIInit_11.8.32.bts, bluez 5.55 and kernel 5.4.142.
I can bring up the BT functionality get hci0 to appear in hciconfig.
I have a gatt server set up and advertising (hciconfig…
Part Number: WL1831 I need some advice about the WL1831MOD module. The antenna layout uses the TI reference design but the ANT016008 antenna is becoming obsolete. To keep using the certification we need to use one of the listed antennas, and the only other…
Hi Andrew,
For this issue, it would be very helpful to have the firmware logs I mentioned earlier in the thread . Was the custom PCB you mentioned delivered?
I can confirm in the firmware calibration can be run based on a temperature change event, but…