I appear to have an error in design which is causing a problem in the manufacturing of prototype. I am not sure if the error is caused by completeness, consistency or incorrect data as it relates to the WILINK 1837 BOM file. Does NA mean not applicable…
Part Number: WL1837MODCOM8I Other Parts Discussed in Thread: TMDXSK437X Tool/software: Linux I use AM437x Starter Kit and WL1837MODCOM8I as reference design with PROCESSOR-SDK-LINUX-AM437X 04.02.00.09.
Could I have dts file to build WL1837MODCOM8I module…
Part Number: PROCESSOR-SDK-AM335X
Tool/software: Linux
Hi,
I was wondering if any versions of ti-processor-sdk-linux-am335x-evm include WiLink 8.7 SP2?
If so, which SDK version(s)?
Otherwise, which SDK version is recommended to install as a…
Saurabh
How can I backport the latest R8.7_SP3 to the 4.14 kernel?
Is it copying the files from git://git.ti.com/wilink8-wlan/backports.git - tag R8.7_SP3 to the kernel 4.14 and rebuild the kernel?
Or is it something else?
What do I have to do…
Part Number: WL1837MODCOM8I Other Parts Discussed in Thread: AM5728 , BEAGLEBOARD-X15 , WL1837 Tool/software: Linux Hello experts,
We have a PCM routing problem while using handfree profile. We have followed the website's instructions and unfortunately…
Hi Hari,
I have done the same compatible and changed the interrupt as high. But still the same problem. The below issue appeared in the log with wl18xx build utilities Update R8.7
[ 20.778051] wlcore: Time Sync: gpio requested
The below issue appeared…
Part Number: WL1801MOD Tool/software: Linux Hi,
I am working on with imx28 processor and I am going to add wl1801mod wifi module to my board. In my board there is only SPI pins are available for connection. So I have made lots of research about the…
Part Number: AM3354 Other Parts Discussed in Thread: WL1835 Tool/software: Linux Hi,
I am using SDK8 tool chain with LINUX 3.14.4 kernel (Beaglebone) in our AM335X Platform.
WL18XX module is integrated to my hardware and i am unable to get the proper…