Part Number: AM62X-PET-CALC Hi TI
For UG1V8_VDDA power rail , current current consumption result is Max current = 100mA, can you help assess whether this is make sense?
If the current is make sense , please help review this power rail layout design…
Part Number: AM62X-PET-CALC
Hi TI
When i finish the PINMUX config and power domain config, there is confict message show as below,Can i suppress these two warning ?
As the MCU GPIO is 3v3 level ,so i connect the VDDSHV_MCU to 3v3 domain.
BR…
Part Number: AM62X-PET-CALC Hi TI
As the data sheet show , E14_RESTATz Pin is low status duing reset, and ss status after reset.
How can i check the SS status of E14?SS:The subsystem selected with MUXMODE determines the output buffer state.
…
Part Number: LM5149-LM25149DESIGN-CALC One customer requested that LM5149-LM25149DESIGN-CALC add notice or cell's limitation or alert if power loss are extremely increased.
When output current and other specs enter severe spec, power loss are extremely…
Part Number: AM625 Hi E2E Team,
I want to calculate power consumption of MMC0 Peripherals in hs200 mode, I was used AM62x power-estimation tool ( AM62X-PET-CALC ) for this calculation, but in spreadsheet for MMC0 = OFF and MMC0 = hs200 mode power consumption…
Part Number: LP-CC2652PSIP Other Parts Discussed in Thread: CC2652PSIP , CC2652P , SYSCONFIG Hello,
In spec and syscfg, I know we can change Tx power as +10 dBm to Zigbee.
Q1: Is there any possible to change CC2652PSIP to +20 dBm?
As for cc2652P…
Part Number: UCC28C41 Hi Team
When using UCC28C41, cusotmer want to know
1.during normal operation, what is the approximate temperature difference between the UCC28C41DR junction to upper surface case?
2. Is there any corresponding application documents…
Part Number: CC2538 Hi,
I have a device designed with the chip of CC2538, NOW have a new requirement, It need to work as a Green Power Combo,
so can you tell me about CC2538 support zigbee green power protocol? or can you recommend a new chip which…
Part Number: TPS92630-Q1 Hi,
As per the Datasheet of TPS92630, the Power dissipation of the IC is as given below. Pls help me understanding the I(VIN). should I consider the quiescent current to calculate the Pd??
If I consider Iq, then i get wrong…
Part Number: C2000-F28004X-POWER-EST-CALC Other Parts Discussed in Thread: C2000WARE Hello,
Please provide a link to document "F28004x API guide" in pdf format
https://dev.ti.com/tirex/explore/node?node=AE-NX3DiUuU.Qi6pGZscVg__coGQ502__LATEST
Thanks…