Part Number: CC1352R
Software: Code Composer Studio 10.0.0 and simplelink_cc13x2_26x2_sdk_4_20_00_35
Harware: CC1352R
In the example application project simple_peripheral_oad_offchip_CC13X2R1_LAUNCHXL, I want to use byte array of big large size…
Part Number: PROCESSOR-SDK-AM62X
Hi,
We developed an app and run on the am62x evm.
I found a problem that there is almost 1 second delay when switch activity(Image).
And the system log always display below log when the activity switched.
How…
Hello Hideaki,
I'm not too familiar with these labs, but I do have a couple of BIOS examples for F28377D that use controlSUITE. These examples use IPC to send messages between CPU1 and CPU2, though, which may be more than what you are trying to do.…
Hi, Attached are the required files for the compiler test case. Additionally, I have created a pdf file where you can see the difference between those two implementations in the disassembly code. I put the macro without the usage of structure in clatask3…
Hi ,
We have our custom J6 board + SDK 7.04.00.03 , but J6 will sometimes come out "serial8250: too much work for irq301" during our production line program.
And then J6 and console will dead . Do you have some advice for this issue ?
Attachment…
Hi Eyal,
Thanks your quick support!!
Please find the details below
1. Yes, I am using the wl_build (R8.7_SP1) to generate the drivers.
2. Yes, Configured in same channel.
3. We were observing the corrupted packets in mesh+AP after around 6 hours…
Part Number: TDA4VE-Q1
Hi, TI experts
HW:TDA4ECO, Customer Board
Our SDK version:
Linux 08.06.01.02
Rtos: 08.06.01.03
BOOT: SBL HLOS boot
We are doing pressure test, 23 seconds power on, 5 seconds power off
The phenomenon I described…
Other Parts Discussed in Thread: ASH Tool/software: TI C/C++ Compiler Hi Team,
I am facing incremental build failure on J721E EVM.Two recipes trying install the same package that is causing issue for us, the recipes are lmbench and mbedtls.
I have…