Dear Pavel,
Thanks for the above pointers, we are looking into it and modifying u-boot and testing,
I have attached two logs of kernel panics,Kindly provide me feedback for the reason for such a panic, It occurs randomly when system runs for more…
Part Number: BQ40Z50 Dear Sir
We have encountered the following problems in the project using BQ40Z50-R1. Please help to analyze them.
Recently, the customer complained about the battery SOC jump in the system, as shown in the figure below. Before…
Hi Khushboo, Sure. Attaching the zip here.
omapboot.txt.txt
Just rename it to omapboot.tar and then just do tar -cvf omapboot.tar
Best Regards, Keerthy
Thank you!
However, I dfo not think project will run just on some EVM without some patches, as the board is our design. Attaching the shematic here.
АКЛС 105 550 001 Плата управляющего модуля с ethernet.pdf.txt
kernel_vulnerabilities.xlsx
Hi [TI Support/Team],
Thank you for your earlier responses and the helpful links.
Just to give you more context — as part of our project security audit, we received a report listing over 4000 Vulnerabilities (we had also…
Hi Samuel,
You are absolutely correct, it looks like the GPO1 row of the sequencer is blank in the latest revision. I've attached a fixed version where it properly controlled by CTL1 and BUCK6_PG again and will update the one on the web. Thank you!…
Dear Team
As I know CRMT revision have being changed to 5.11. We use lot of TI IC product in our product . And our customer request us to provide the TI CMRT revision 5.11 form(file attached) Could you help me to reply the questions in the form?? (or…
Other Parts Discussed in Thread: AM3352 Hello all,
Currently I am working on AM3352 processor and I want to use DDR3 RAM.
In datasheet of AM3352 in section 7.7.2.3 they are mentioning that if 16 bit DDR3 is used then termination is not mendetory.…
Part Number: TMS320F280049
Tool/software: TI C/C++ Compiler
I am getting this error when I call a function via function pointer in .cla file which is defined in a structure. The function pointer has been assigned the address of function in main()…
Part Number: DRA72 Tool/software: Linux the carlife already connected success,but still occur EAP write timeout when use the IF 3,then I use USB logic analyzer to capture data,result indicate the last data do not sent out.
attachment is a related log…