Part Number: BQ41Z50 Other Parts Discussed in Thread: BQSTUDIO , BQ41Z90 Dears,
The IC that has already been programmed with firmware cannot be programmed again. Programming firmware to a new IC can be successful.
Even the demo provided on the official…
Part Number: CC2340R5 Tool/software: Hi,
We will develop a ble module for our devices and use CC2340R5.
Unfortunately, we have iar 8.40 and could not renew it at this time. How can we program and debug in our version of IAR?
All the bests,
Sa…
Part Number: LP-EM-CC2340R5 Other Parts Discussed in Thread: CC2340R5 , SYSCONFIG , UNIFLASH Tool/software: Issue Description: When we perform a scan using BTool and our scanning device initiates a connection, the connection is immediately dropped within…
Part Number: CC2340R5 Other Parts Discussed in Thread: UNIFLASH Hi,
In our project, we use the CC2340r5 and we have a custom bootloader which has 60 sectors of flash dedicated to it, the application then uses the other 206 sectors of flash.
We have…
Part Number: CC2340R5 Other Parts Discussed in Thread: UNIFLASH , LP-XDS110 , CCSTUDIO Tool/software: Debugging is not allowed. If this is not expected, check your CCFG. If you are experiencing issues with loading your application, do the following (this…
Brennan Hartigan said: Kier is incorrect in that TIDA 01606 can absolutely be used with TMDSCNCD263
Apologies Brennan, I actually misread your post! I'm intrigued. So the F2837xd control card is HSEC pin compatible with the TMDSCNCD263? If so, where…
Part Number: CC2340R5 Other Parts Discussed in Thread: UNIFLASH Hi Ti,
I want to use data stream firmware: GitHub - TexasInstruments/ble_examples at simplelink_low_power_f3_sdk-7.20
I find there is no .hex and .out file after I build the application…
Part Number: TMS320F28P650DK I am facing this error "C28xx_CPU2: File Loader: Verification failed: Values at address 0x00A840@Program do not match Please verify target memory and memory map. C28xx_CPU2: GEL: File: C:\Users\saini\workspace_v12\epwm_ex4_deadband…
Hello,
zhang tao said: Why is it that when using the emulator for debugging, the encryption is successful and the code can run
Did you perform an ECSL or CSM unlock when running the application with the DCSM enabled? If you only do a ECSL unlock,…
Part Number: CC2340R5 Tool/software: Hi Team,
My customer try add NVS in basic_ble project.
We follow the instructions by the E2E thread to modify basic_ble.syscfg and ccc23x0_app_freertos.cmd. But it still not worked.
https://e2e.ti.com/support…