Part Number: LM2673
Tool/software:
Hello
I would like to control a buck converter with 18V positive output and a boost converter with -18V negative output using digital potentiometers.
The input is 20V and I need some help deciding what would…
Part Number: DDC3256 Tool/software: Dear TI team,
We would like to design data acquisition system with DDA2256 A / DDC3256.
Could you please let us know if either of the device is available in chip on Flex package.
And, also share the full datasheet…
Part Number: RF430CL330H Tool/software: Hello,
I have been trying to find a solution to replace a traditional rotary coupling for control signals to a couple of sensors for a robotic arm. The existing rotary couplers are basically electrical wipers…
Other Parts Discussed in Thread: LDC1051 , LDC1312 , LDC1612 , LDC1614 , LDC1314 , LDC1101 Dear Sirs
Is LDC1051 NRND?
Do you recommend other Inductance to Digital Converter solution?
BRS
Nat
Part Number: TMS320F28027F Tool/software: Hello, expert When we used the F28027F to control the induction motor, we found that in the motor parameter identification process, the value of Rs identified was extremely large (approximately up to 2.3e23).…
Hi Haydar,
Sorry for the delay.
HAYDAR BILHAN said:
We do not necessarily need the A/D conversion of the baseband signal at 3MHz, but rather the envelope or the RMS value of it.
This should work fine.
HAYDAR BILHAN said: We are concerned capacitive…
Hi, We are going to measure AC Voltage directly by external ADC.
AC Voltage input range is 100mV to 1V RMS @50/60Hz.
Kindly suggest suitable TI part number.
Regards,
Mohan
Sayali,
Please take a look at the LDC1314 inductance-to-digital converter evaluation module: 1-degree dial EVM and its user's guide . The LDC1314 is very similar to the LDC1614 so this EVM should provide some guidance for your design.
Regards, Jo…