Part Number: TPS92662-Q1 Tool/software: To Whom It May Concern,
I have a question regarding the PWM range of the TPS92662-Q1.
The TPS92662's PWM is a 10-bit system for dimming, meaning it has 1,024 different levels of brightness, but the PWM frequency…
Part Number: TMS320F28379D Tool/software: I have generated the phase-shifted PWMs of 100kHz for Phase-shifted Full bridge application.
during testing in open loop, at 100V hv input to PSFB, the phase-shifted PWM pins' frequency change to 200kHz.
This…
Part Number: TPS92201 Tool/software: Hi,
I have designed new ledpanels with tps92201 for driving an individual farred led.
Now it works for 99%, but the led always is on, also when PWM=0.
Enable pin is connected with VDD (5V).
How can i turn…
Part Number: TIDA-010938 Tool/software:
in the design program file run lab 1 but if not "(stringINV_clearPWMTripBoost == 1U) " not show open loop and closed loop PWM in any LAB so, these variables not set in any placed so its reset or set to 1, and…
Part Number: PMP23338 Tool/software: Hi all
I am following the guideline of PMP23338 ( https://dev.ti.com/tirex/explore/node?node=A__ANlQ.5FNEOWS7jYnIynC-g__digital_power_c2000ware_sdk_software_package__5C6SEVO__LATEST ) and trying to run builds/labs…
Part Number: J722SXH01EVM Tool/software: Hello,
I need help with the PWM enabling process. If there is any documentation or reference guide that helps with this process. Please provide the link.
Part Number: DRV8703-Q1 Tool/software: Hello ,
Now ,we are use DRV8703QRHBRQ1 to control motor , use PH/EN mode (Mode=0), and the PWM frequency is 20KHz. but we have one issue , input PWM signal from IN2/PH but find the output PWM signal fixed is 20…
Part Number: TMS320F2800137
Tool/software:
Hello, I am using the official routine of 137 and want to use my own hardware. C:\Users\Lenovo\Desktop\test\universal_motorcontrol_lab_f280013x On the hardware side, the MOS is directly driven without SPI…
Part Number: TPS923652 Other Parts Discussed in Thread: TPS92641 Tool/software: Hi Sirs,
I want to confirm the speed at which the LED driver can turn on and off the IRLED current.
Do boost and buck-boost modes have the same performance?
I expect…
Part Number: DRV8702D-Q1EVM Other Parts Discussed in Thread: DRV8702-Q1EVM , , MSP-EXP430G2ET , DRV8702-Q1 Tool/software: I found the DRV8702-Q1EVM board very suite for controlling inductive loads in general. Currently, I am controlling the board using…