You have to load the sample programs (modify to your taste) to find dead band don't work the same when 2 or even 3 PWM generators are configured.
That is 2 or 3 phase commutation dead band cycle then requires special handling the example single generator…
Richard Bland said: The TivaWare Boot Loader User Guide does not even mention ROM_UpdateUART(). Agree that TivaWare" Boot Loader USER'S GUIDE SW-BOOTLDR-UG-1.0 doesn't mention ROM_UpdateUART. However, my understanding of the TivaWare Boot Loader User…
sorry for the delay
All Stellaris MCU SWU is available through www.ti.com/stellarisware
you can download the whole thing or specifically for the DRV8312 kit:
http://www.ti.com/product/sw-dk-lm3s-drv8312
There was an issue on the 22nd where…
Huy -
After you raise the EN line, did you verify that your 13.56MHz crystal is running? also - you can check the Bandgap voltage which should be 1.6VDC.
If you are using the LM3S line of Stellaris MCUs, then i would recommend that you go request…
Q: How can i approach for the kit i have (DK-LM3S-DRV8312 and LM3S818 MCU) ?
A: follow DRV8312-C2-KIT controlSUITE C:\ti\controlSUITE\development_kits\DRV8312-C2-KIT_v124\BLDC_Sensored
Q: I have to add a hall_drv module in the feedback loop?…
Os Version: Linux Ubuntu 10.4 LTE 32 Bit
Uname -a : 2.6.32-46-generic #108-Ubuntu SMP Thu Apr 11 15:55:01 UTC 2013 i686 GNU/Linux
CCS Version: 5.4.0.00091
Licence: limited version both MSP and ARM (buy full licence planned later if all processor…
Hello Amit,
Thank you for your prompt and helpful reply.
I have a few additional questions relating to your answers Bolded below.
“1.a For Port F APB aperture it is correct. For AHB it is not correct”
I understand this answer. No questions …
Other Parts Discussed in Thread: SW-DK-TM4C129X , TM4C129XNCZAD Hi,
Why does viewing datasheets of the TM4C129x series of microcontrollers require a click-thru NDA? Neither the TM4C123x series or much more complex processors like the AM335x line require…
cb1- said:
Kindly perform the detailed test as described. In addition - as you report only cmos USART levels - with what external device does your USART transact? And how do you judge correctness of transfer? Can you - in any way - monitor data and…
"Happy new year to you too, Pete. You prove a most welcome new (contributing - not just taking) addition to this forum."
I do like to given back more than I consume. I also like to provoke people into thinking for themselves and being the creators…