How long will this components be in production before it go obsolete since I saw the last it was in production 5 years ago based on some posted.
How long will this components be in production before it go obsolete since I saw the last it was in production 5 years ago based on some posted.
Hey ttd,
I took a closer look at the ADS8515 and with the difference in reference voltage and internal resistors, its offset is better than the ADS7805. The main source of error there is with the internal reference. The ADS8517 has better offset as I…
hi
i am trying to oversample ads8517 adc ic to get high resolution result basically i am trying to implement a adc and dac calibration system i have seen delta sigma adc but sample rate is very slow and accuracy…
Hi Andy,
Does the application still require the 50kHz input bandwidth? If so, take a look at the following devices:
16-Bit, 250-kSPS, 1-Ch SAR ADC with programmable (±10/±5/±3.3V) input ranges and SPI interface:
http://www.ti.com/product…
As you have stated before I used to work with complete front end type ADC, They can read output up to 10kg. Which is unnecessary for me. I must obtain 200000 noise free counts. That's why I guess I was not successful.
Actually I need much lower…
This technical article was updated on July 23, 2020.
Did you know that the input signal might affect how you select the best successive approximation register (SAR) analog-to-digital converter (ADC) for your application?
When we hear the word, “input…