Hi All,
Is there a power supply sequence for VA and Vref when powering up?
Thanks in advance.
Regards,
Toshi
Hi All,
Is there a power supply sequence for VA and Vref when powering up?
Thanks in advance.
Regards,
Toshi
Hi team,
is there any Alternative part like DAC121C085 but with Nonvolatile Memory, better also has 9 I2C address as well, thanks.
Hi,
I see that the full-scale error in the data sheet is -0.1 %FSR typical, and -0.7 %FSR maximum.
This might be basic, but I'm confused by the negative sign. Does that mean the error will always be less than the "true value"?…
Hi,
Is there an advantage in noise performance of connecting VA and VREF to the same supply?
Any ratiometric advantage of having those two supplies being the same and hence moving together?
Or is the noise performance solely based…
Hi Paul,
Thanks for your support.
For DAC121C085 support for external reference voltage.
So we used Noise free 2.5V regulator output (LP2980) connect to the DAC VREF pin 7.
Need your help to understand the below points since i could not find application…
What is the default value for DAC register? I'm using it with external reference source of 2.5V.
I couldn't find it on the datasheet
Thanks,
Khoi
Hi,
I am trying to use DAC121C085 with xtr116 for 4-20mA output. I saw a design for DAC8551 with xtr116 and DAC8551 has a RC circuit which connected to Vref of XTR116. Is that needed…
Hi,
I am trying to use DAC121C085 with msp432p401R and i need an example code. Is there an example code ? Thank you.
Hello team,
Could you kindly help to share the link of the GUI of DAC121C085 Evaluation ?
Thanks,
Antony
Part Number: MSP432P401R
I am trying to use DAC121C081 with msp432p401R. but at debug mode software stucks at while (I2C_isBusBusy(EUSCI_B3_BASE));
int main(){ Init_I2C_GPIO(); I2C_init(); I2C_setslave(0x0C); I2C_write16…