Tool/software:
We use the DP83848I. The design is created according to the guidelines.
The power supply is a stable 3,3V. and the IC has a RMII interface to an STM processor.
On other side it is connected to an RJ45 connector with…
Tool/software:
We use the DP83848I. The design is created according to the guidelines.
The power supply is a stable 3,3V. and the IC has a RMII interface to an STM processor.
On other side it is connected to an RJ45 connector with…
Tool/software:
Hello,
I have a question regarding the DP83848IVVX/NOPB.
I am currently designing hardware with the DP83848I using the RMII interface.
Could you please review the attached schematic? I would appreciate it if you could…
Hi Joey,
The team hasn't done any center tap combinations other than the datasheet's recommendation. Any difference from the recommended configuration puts validation responsibility on the customer.
The customer is welcome to explore if this RJ…
Tool/software:
The LED_ACT/COL of the DP83848 is not functioning.
It remains in a HIGH state continuously.
Other LEDs are working properly.
Case 1) When reading PHYCR (0x19, 0d25), the value is 0b1100010111100001.
bit6 (LED_CNFG[1…
Tool/software:
Hi Team,
Does DP83848 support the following function?
There are no described in the data sheet.
1) WoL (Wake-on-LAN)
2) Cable diagnostic
3) Rapid link down detection
Best Regards,
Tool/software:
Hi Team,
The typical supply voltage of DP83848 is 3.3V, with 100BASE-TX, what is the max value of Idd? There is only the typ value on datasheet.
Thanks
Best,
Frank
Tool/software:
Hi team,
After this chip is used for a period of time, the data rate of some products will be reduced, and the network speed will only be 1-2M. How to do a loopback test of DP83848?Thanks.
Hi Alvaro
Thank you. We currently have a way to improve the soldering a little with a special solder.
If we need tin-plated components again, who could we turn to?
Unfortunately, the NiPdAu surface is not a good option for us.
Thank you.
Hi Evan,
Thank you for your respense.
I steel have problem, d'ont work for me but I've noticed that to configure the DP83848I-MAU-EK for SNI mode, we need to set the following pins:
And also :
Hi Alon,
Thanks for confirming. We have shared feedback over email.
Best Regards,
Evan