I'm using a TM4C1232D5PM and a W25Q64 SPI FLASH memory.
I read blocks of 8,192 bytes from the memory. Depending on the contents of the 8K block the SPI clock will get stuck low. I have tried different SPI…
I'm using a TM4C1232D5PM and a W25Q64 SPI FLASH memory.
I read blocks of 8,192 bytes from the memory. Depending on the contents of the 8K block the SPI clock will get stuck low. I have tried different SPI…
I am trying to communicate ti’s TM4C1232D5PM (ARM Cortex M4 based) as a master and linear’s LTC2983 as a slave by SSI protocol.
I have used SSI2 module for interfacing, port PB4,PB5,PB6,PB7 is used…
Hello
I am working on Ek-TM4C1294Xl launch pad board.
I am able to work on the launch board easily but when I try working on my target board I fail to do so. I am unable to transfer the program…
For others facing an issue where previously- working hardware designs now fail in the board-programming process:
The updated Tiva/Stellaris DFU Windows driver supplied in the recent "XDS-IC…
The Boot Configuration Register (BOOTCFG) refers to ROM Boot loader and how it starts.
I'm using a TM4C1232D5PM and on the very first power up the boot loader will execute automatically. It will also start if you erase the entire FLASH memory.
In…