Helmut,
I would not worry much about the discrete syncs if bt656 embedded syncs are being used.
The line below and the attachement may be of help. VPIF reset after disconnect is discussed. It is possible that during your start up sequence, capture…
Part Number: TPS51285B Other Parts Discussed in Thread: CSD87350Q5D Dear Sirs,
My customer is testing with TPS51285B and want to set up the OCL with attached excel tool.
However, with the result of tool, it seems the OCL value is very large than…
Hi Adam
attached the only two TMS320C28x Optimizing C/C++ Compiler User's Guides (v6.2 and v6.2.4) published before v6.4.
spru514f.pdf
spru514g.pdf
Regards, Bernd
Hi,
i am using IPNC dm8127.i tried NFS boot but it is not streaming through rtsp links.and also i faced the jffs2 file system error
this is my bootargs
setenv bootargs 'console=ttyO0,115200n8 root=/dev/nfs rw mem=80M vram=4M notifyk.vpssm3_sva=0xBFD00000…
I have solved the former questions, thanks for your help.
Recently I am doing an experiment that I input an Mpeg2 file first, decode it to yuv format and then encode it to H264 format. The MPEG2 decoder is got from TI, while the h264 high definition…
Part Number: LP-EM-CC2340R5 Other Parts Discussed in Thread: LP-XDS110ET , UNIFLASH , CC2340R5 Tool/software: I used the LP-EM-CC2340R5 and upgrade the Host Test code. I found that he TX power default value is 8 dBm.
I try to remove the “Custom” option…
The EVM was never designed to meet any kind of PFC requirement so my slightly educated guess would be somewhere between 0.3 and 0.5, especially considering the input capacitor is relatively large to keep the input ripple on the bulk voltage within 25…
Hi Vamsi,
The call tree info makes sense. I seems the linker is automatically minimizing the amount of the library which is being inserted into the final image.
I think I got the file inserted now. I changed the extension from zip to txt.
CM_Link_Error_Zip…
Hello:
I information and you give me a link error is not the same.
I try to do the following:
$ strace -o log opkg install dlp-sdk_2.0-r8.0_cortexa15hf-neon.ipk
1768.log.txt
View the log file found that there are several directories not created…
hi Sanjeev
1. the telnet is ok.
2. ther is pm enable
3.rev of the mistral boaed is rev D
4.the .config:
# # Automatically generated make config: don't edit # Linux kernel version: 2.6.29-rc3-omap1 # Thu Mar 4 10:45:04 2010 # CONFIG_ARM…