Part Number: TDA4VM
Hi,
When we use the prebuild image of Linux Kernel provided by TI, the system have the ability to automatically insmod the Linux Module.
When we use the source code (board-support\linux-4.19.94) provided by TI to compile the…
Tester_HCILib.xml Hi Joakim,
I think you required below setting for scanning device right ? along with this i am also attaching xml file of commands that i use
12:26:33.555 --
12:26:33.555 Packet "HCI_EXT_ResetSystemCmd", Opcode 0xfc1d
12:26:33…
Hi Experts,
We are running an application which send the http request/http response packets to/from the server (AWS server). The issue is request response is taking too much time and TCP server is initiating transmission packet. PFA is the pcap files…
Other Parts Discussed in Thread: WL1271 Hi,
I have problems bringing up wl1271 interface. I have kernel 2.6.35 and compiled wl1271_sdio as module. When I start wl1271 interface ("ifconfig wlan0 up"), I see the driver sending the firmware and booting…
Part Number: TDA4VM Other Parts Discussed in Thread: SYSBIOS , CSD Hello,
We have an issue with the IPC driver on QNX. When big data is being sent (for reproducing error we used 496 bytes) the TI IPC resource manager seg. faults.
This happens once…
I ran it from 0 and scanned through 1300 entry, 0 to 36 were corrupt...
Debug: save_byte(204, 0) saved the value 204 to 0 in ext_flash Debug: save_byte(204, 1) saved the value 204 to 1 in ext_flash Debug: save_byte(204, 2) saved the value 204 to 2 in…
Here is a full CE_DEBUG=3 trace. I think you're right about the free happening on a size. Hopefully, this will help you debug.
Creating VCA
@28,501,225us: [+0 T:0x43e0b490 S:0x43e0a094] ti.sdo.ce.vidanalytics.VIDANALYTICS - VIDANALYTICS_create…
Other Parts Discussed in Thread: WL1271 , WL1283 , TPS65910 , DA8XX Hi All,
I am trying to debug Bluetooth in my custom board based on am335x starter kit.
We have replaced wl1283 with wl1271 in our custom board for future GPS support.
We are using…