Part Number: ADC3444
Dear Forum members.
We are having some trouble with unwanted noise on the input of the ADC.
With absolutely no input signal connected to the input of the ADC only the passive input filter.
we are measuring noise with the oscilloscope…
Part Number: ADC3444 Other Parts Discussed in Thread: ADC3443 Hello,
My team has chosen ADC3444 for IF sampling application for a 25kHz BW signal. We will use it for 1-wire LVDS configuration, i.e. 80MSPS max. I would like to know if this Quad-Channel…
Part Number: ADC3444 Hello,
We want to interface the ADC3444 with a FPGA Ultrascale+ from Xilinx. The ADC work in 2 wires mode with a frame clock which encapsulates 2 samples.
We saw the application note from Xilinx which describes a deserialization…
Hi Nick I'm not familiar enough with the Sitara evaluation module to know what high speed ADC EVMs might be compatible. I am going to re-direct this question to the TMDSEVM572x experts to see if they can provide any additional information regarding which…
Part Number: ADC3444 Other Parts Discussed in Thread: ADC3244 We think that it is fine, but there seems to be a bit of an issue with the ADC344x Datasheet SBAS670B –JULY 2014–REVISED APRIL 2017.
Table 7.12 seem to have a couple of typo’s in it:- …
Part Number: ADC3444 Does the ADC3444 consists of the frame clock pattern? how to rearrange the frame clock while coming from the pcb? is there any application notes available related to this topic? thanks in advance
Part Number: ADC3444 We see that the datasheet says that synchronisation could cause glitching on the clock:-
On the ADC344X we have two output clocks: DCLK and FCLK. It is not clear from the datasheet which of the clocks is affected by the…
Part Number: ADC3444 Other Parts Discussed in Thread: AM5728 , , TLK10081 , ADS58H43 , ADS5263 Dear Team,
One of my customer want to use a high speed ADC (ADC3444 with LVDS serial interface) with the processor AM5728.
AM5728 has not an integrated…
Part Number: ADC3441 Other Parts Discussed in Thread: ADC3444 , ADC3444EVM , LMH5401 I want to use ADC3444 to digitalize a wide bandwidth analog signal with single polarity from -0.2V~1V. As described in datasheet that "Each input pin (INP, INM) must…